Skip to main content

VMD business centre

Zagreb, Croatia

bg-image

At just over 96m tall with 25-storeys, VMD Tower B is the tallest office building in Croatia, and one of the most efficient, earning an "A energy certificate" for its green building practices. With 19,800m2 of floor space, consisting of offices, corridors and a gym on the ground floor, our VRV IV ensures the entire premises maintains the perfect climate.

A total climate solution

bg-image

To achieve the best in climate control and energy efficiency, we installed 57 outdoor units on the roof of the building to serve 685 ceiling cassettes. Using Variable Refrigerant Temperature technology, VRV IV can continually adjust the refrigerant temperature to match heating and cooling demands of the building, while lowering the total energy consumption. By integrating heating, cooling and ventilation into one system, we dramatically improved the building's energy efficiency, lowered its carbon emissions and earned more energy savings.

Our VRV IV is also an ideal system for buildings such as VMB Tower B that need to manage multiple tenants. Through this system, tenants can manage their own climate zone and receive billing for only their energy usage.

Solution at a glance

bg-image
  • 57 VRV IV heat pumps
  • 685 round flow cassettes
  • 2 Intelligent Touch Manager units for central control and billing

Learn more

Our other cases

  • A high efficiency solution for a residential building

    This residential project was executed in the context of the renovation of a residential building, which had energy efficiency as a main aspect.
  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • Biocoop

    Daikin completes the installation and commissioning of the first transcritical CO2 refrigeration solution on the French market at a meat processing laboratory in the Dordogne.
  • Bringing Air Conditioning in stadiums

    A Daikin R-32 chiller has recently been installed and commissioned in a HVAC project involving a stadium in Sittard, in the Netherlands.
  • C&A

    Looking to renovate its entire HVAC system, the C&A store wanted to achieve year-round comfort in the most cost-effective and efficient way.
  • Cha No Ma

    Air purification with advanced streamer technology complements Daikin’s environmentally friendly R-32 systems to create a comfortable and healthy café experience.
  • A Chiller Solution For A Complex Of Office Buildings

    Daikin has recently provided its chiller solutions for an office building project in Krakow, Poland.
  • Chillers with R-32 refrigerant at Heinzinger electronic

    An air-cooled chiller from Daikin with a scroll compressor and an output of 200 kW is used, which for the first time works with the climate-friendly refrigerant R-32 and is characterised by optimal operating behaviour and high energy efficiency.
  • City Centre Hotel

    Chiller change boosts comfort at central London hotel.
  • Claerhout Office

    Advertising agency Claerhout Communication House opted for our VRV IV total solution for their new open landscape office building which provides office space for 45 employees and a conference room for 150 guests.
  • Providing a complete HVAC system for a food processing plant

    Daikin recently supplied a complete HVAC system to meet the cooling needs of a food processing plant in Hungary. The end user operates in the supplements business, producing plant-based supplements including vegan proteins.
  • Conversion of an old R-22 system

    Conversion of an old R-22 system to a VRV 5 S-series with R32 refrigerant
  • Cooling and heating for small residential buildings

    Daikin BLUEVOLUTION heat pumps installed in a residential project in Porto, Portugal, offer high energy efficiency with 21 kW cooling and heating capacity.
  • Cooling concept for the Engelbert Strauss CI Factory

    Low CO2 footprint and a climate-friendly overall cooling concept for the Engelbert Strauss CI Factory.
  • Coral betting office

    Discover how our auto-cleaning roundflow cassettes achieved 50% more energy savings for Coral betting offices.
  • Courtyard Hotel Paris

    The Courtyard conversion marks a successful collaboration between forward- looking urban regeneration and Daikin’s flexible, future-proof VRV heat recovery technology.
  • Crédit Agricole

    Known as "the green bank" due to its agricultural history, Crédit Agricole wanted an energy efficient and low maintenance air conditioning solution for one of its branches.
  • Crystal Tower

    To help Crystal Tower maximise its energy efficiency, we planned to combine the power of air-cooled VRV, water-cooled VRV and chillers to deliver an all-in-one climate control solution.
  • Customised air conditioning for shopping centre

    Read about a complete solution by Daikin for the Intro Bergheim shopping centre with 22 retail units in the centre of Bergheim near Cologne
  • Daikin Emura, design solution for residential living

    Let’s take a look around this apartment in the centre of Milan, Italy’s renowned design and fashion capital. Did you notice the new white Daikin Emura on the wall? It’s an elegant design that beautifully blends into the interior.
  • Desco showroom

    Daikin’s ‘plug and play’ rooftop system offers sustainable year-round climate control solution for customer showroom
  • Efficient and reliable technology

    Daikin screw inverter chiller technology’s worth has been proven again in a HVAC project involving another major pharmaceutical company.
  • Energy efficiency

    Daikin has recently provided HFO screw inverter chiller technology solution to major pharmaceutical company for one the manufacturing sites in Wien, Austria.
  • Extending the Daikin L∞P programme

    Daikin Applied Europe has recently extended its L∞P programme to chillers, using certified reclaimed R-134a refrigerant for chiller ranges that are charged by the gas.
  • Extension of the L∞P programme by Daikin to chillers

    Daikin Applied Europe has recently extended the L∞P programme by Daikin to chillers. Thereby, Daikin is the only manufacturer actively promoting and supplying units with reclaimed refrigerants, for a wide range of products, from screw and scroll compressor units to centrifugal compressor machines.
  • High energy efficiency for comfort cooling in Middle East conditions

    Daikin has recently supplied chillers to provide comfort cooling in Middle East conditions in a project involving a four stars hotel in the city of Riyadh, in Saudi Arabia.
  • Holcim cement plant

    The Holcim cement plant relies on state-of-the-art technology to achieve its ambitious environmental and energy-efficiency goals.
  • Residential property with home office

    Building a new residence with an all-round climate control solution
  • Hotel St. Annen

    Located in a quiet residential street in central Hamburg, the Hotel St Annen creates a warm and welcoming ambience for visitors in modern surroundings.
  • Hoteles Santos • Las Arenas

    The Daikin VRV replacement system was the perfect solution for a system upgrade to reduce the energy consumption while keeping the hotel business uninterrupted.
  • Ibis Budget Hotel, Ghent

    In March 2018, the new IBIS budget hotel opened its doors at the Dampoort in Ghent, offering guests outstanding comfort in a modern attractive setting. For the building owner Viktor De Maertelaere, investment in an energy efficient and reliable climate control system was key to the budget hotel concept.
  • Immogra

    Daikin’s VRV IV system delivers modern aesthetics with invisible integration of HVAC.
  • Is R-32 really losing relevance in the refrigerant game?

    Learn why R-32 remains a sustainable option in HVAC, despite growing attention on R-32 blends and low GWP refrigerants.
  • JBC

    In its ongoing search to optimise running costs, JBC conducted a site trial with Daikin designed to evaluate the gains generated by Variable Refrigerant Temperature (VRT) technology.
  • JBC K'dee

    JBC entrusts optimal climate management for the first innovative experience shop for children to Daikin.
  • K-Way

    When high-end clothing retailer K-Way opened a new store in Covet Garden, London, we worked with nation-wide D1 contractor Royale to devise and install the perfect energy-efficient solution for the property.
  • L1 DOT Complex Poland

    Daikin teams up with building designers to maximise BREEAM* rating with its commercial heat pumps
  • Leon's restaurant

    M&E contractor, Synecore, installed its first ‘invisible’ HVAC system, the Daikin VRV IV i-Series at Leon Restaurant, central London, to overcome tight space restrictions and achieve maximum climate control efficiency.
  • LOOP by Daikin Toyota

    Czech Toyota Motor Manufacturing makes a sustainable choice by joining circular economy program L∞P by Daikin
  • Making hospitals more efficient

    Daikin has recently taken part in an important project involving hospitals in Istanbul, Turkey. It is a government project, aiming at making hospitals more energy efficient through the replacement of chillers and other components of the HVAC system that provide these buildings with cooling or heating.
  • Meeting a hospital’s cooling needs and keeping power input low

    Daikin has recently provided chillers for one of the biggest private hospitals in Qatar. The hospital has world-renowned international affiliations and the mission to provide optimal patient care by utilizing unparalleled and advanced services.
  • Merlin Properties

    As part of a business center in Madrid, this office complex was upgraded to a more efficient solution, while keeping investment costs under control.
  • Naturkost Brinkman

    Organic specialist retailer Naturkost Brinkman uses Daikin retail refrigeration to deliver improved energy efficiency and in-store comfort.
  • New office building for hotel outfitter TKS in Borken

    Daikin provides heating, cooling and ventilation for hotel outfitter TKS in Borken
  • Office refurbishment in Madrid, Spain

    Daikin’s VRV 5 S-Series provided the ideal solution for a refurbishment project of a semi-detached villa in Madrid
  • Perial Asset Management

  • Pomme d'Or Hotel

    Air conditioning has become the norm in most new and refurbished hotels. Today’s systems keep guests cool during summer – and additionally provide cost-efficient heating during winter periods. Daikin heat pumps use renewable energy to do this, cutting hotel operating costs. And there’s also a positive impact on indoor aesthetics.
  • Hotel Santos Porta Fira

    The Santos Group, the organisation in charge of building Porta Fira, selected Daikin as a trusted partner to deliver a unique, reliable and energy-efficient climate control system for the building.
  • The Post Hotel

    As climate control specialists, we chose our VRV system for the Post Hotel Ghent for its combination of energy-efficient technology and ability to provide more comfort.
  • Prezzemolo & Vitale - Palermo

    For the new Prezzemolo & Vitale store in the historical centre of Palermo, a system was installed consisting of Daikin Zeas and VRV units.
  • Providing cooling & heating for small residential buildings

    Daikin integrates BLUEVOLUTION heat pumps and solar kits in residential projects, providing efficient heating, cooling, and hot water with the R-32 Small Inverter Chiller.
  • Providing cooling for an industrial manufacturer of automotive components

    Daikin supplied a 307 kW air-cooled screw inverter chiller to an automotive parts plant in Lisbon, providing efficient cooling and remote monitoring with Daikin on Site.
  • Radisson Blu and Proximus

    The new Radisson Blue hotel in Bruges is located near Bruges station, an area which has seen extensive redevelopment over the past few years. Built by Belgian property developer Group GL, the impressive new tower complex houses not only the new hotel but also a 6,000 square metre area of office space, currently occupied by GL tenant Proximus.
  • Hotel Reina del Mar

    Hotel Group HVD sought a total climate control solution for its first ever luxury beach complex on Bulgaria’s Black Sea Coast.
  • Samrya 44

    With 44 floors of elegantly-designed luxury suites, Samrya 44 adheres only to the highest standards in construction and HVAC.
  • Daikin's AHU solutions for an interesting HVAC project

    Daikin has recently provided its AHU solutions for an interesting HVAC project, which have been executed in Lanheses, Portugal.
  • Sound enclosure case study in Flassy

    The acoustic effectiveness of Daikin’s new Sound Enclosure for its Sky Air and VRV 5 outdoor units has been validated by field trials undertaken at a residential installation in Burgundy, France, showing significant sound reductions equal to and even exceeding factory test room values.
  • Sportisimo

    For this project, we chose to install an outdoor system that connects to a variety of indoor and ventilation units strategically placed in the shop.
  • The Bloomsbury Hotel

    The VRVIII Heat Recovery System from Daikin was selected for its supremely low energy consumption and ability to off er massive savings in comparison with similar systems
  • The food Air is also at star level in the Restaurant „La Cuisine Rademacher“

    The restaurant “La Cuisine Rademacher”, founded in Cologne in 2018, was recently awarded a star by the Michelin Guide. Due to the pandemic and the associated lockdown, the restaurant can currently only offer a take-away
  • The new Small Inverter Chiller providing heating for a public swimming pool

    Daikin has recently supplied two new Small Inverter Chillers with R-32 (in the heating version) as a replacement for the old heat pumps at the Public Swimming Pool of Vila Pouca de Aguiar in Portugal. The new units will complete the pre-existing HVAC system.
  • Torre Serenissima

    Equipped with an outdated R-22 refrigerant system, we gave the Torre Serenissima a full upgrade to deliver more energy efficiency and comfort.
  • Training Centre Belgium

    Daikin sought a future-proof low energy HVAC solution for its new Training Centre located in Ghent.
  • Turkmenistan Success Story

    Daikin has recently provided it’s a complete HVAC solution for a mixed-use complex, which will be the largest shopping and entertainment center in Aşgabat, the capital of Turkmenistan.
  • Van der Valk Hotel

    From the lobby to the guest rooms to the kitchen, every space in the Van der Valk Hotel has its own unique climate needs. Our goal was to develop an integrated system to meet the needs of each of these locations and lower the total environmental impact of the system.
  • Velocity office building

    Sustainability is at the forefront of Velocity's design. Each element of the design has been carefully considered to ensure an EPC rating of "B" and an "Excellent" BREEAM rating has been achieved.
  • Venetian Arsenal

    An innovative climate control system that taps into the natural energy of the Venetian Lagoon is delivering high levels of comfort and energy efficiencies while preserving an historic industrial building in the heart of Venice.
  • VMD business centre

    A VRV IV system is providing all the heating and cooling for VMD Tower B, a 25-storey office building in Zagreb, helping it to meet the highest levels of efficiency and lowering energy consumption.
  • VRV heat pump contributes to low carbon footprint

    The new Arteparc commercial complex situated in the Inovallee techpark in Meylan, Grenoble demonstrates how developers and equipment manufacturers are working together to deliver new lowcarbon buildings that align with the highest standards of sustainable development.​
  • Warm pool water through heat recovery

    State-of-the-art Daikin integrated heat recovery technology saves a significant amount of energy and heats the water in the hotel's pool.
  • What to consider when choosing a heat pump for a residential building

    Daikin heat pumps and R-32 Small Inverter Chillers offer energy-efficient heating, cooling, and hot water for residential buildings, reducing CO2 emissions with a compact design.
  • Zome

    The hubs from ZOME are modern and agile spaces to offer a personalised experience to customers.
  • UAE Police

    Providing a cooling solution for an office building in the UAE

    Daikin recently supplied four chillers for the Headquarters of the Emirates police force, in the UAE. The chillers will be used to provide cooling through air handling units through the large building and ensure the maximum level of comfort for occupants.
  • hospital in Oman

    Supplying a hospital with an efficient, reliable, and compact solution

    Daikin recently supplied a chiller for a big hospital in Oman. The hospital’s capacity was extended with the opening of a new wing, which required the HVAC system to be integrated with a new chiller to meet the greater cooling needs of the building. For this project, it was essential to find a reliable solution with advanced technology that could perfectly meet the needs of the facility.
  • Providing cooling for the High-Luminosity LHC project at CERN

    Daikin recently supplied 8 water-cooled chiller units to CERN to provide cooling for the High-Luminosity LHC (Large Hadron Collider) project. The High-Luminosity LHC project aims to boost the performance of the LHC to increase the potential for discoveries after 2029. The goal of the project is to increase the integrated luminosity by a factor of 10 beyond the LHC’s design value. That will allow the gathering of a higher quantity of data and observations of rare processes as the increase in luminosity will make the LHC more powerful.
  • Hotel in Las Arenas, Valencia

    Las Arenas

    When it came to upgrading existing VRV systems to reduce maintenance costs and further improve comfort control, choosing a replacement solution with lower CO2 footprint was top of the agenda.
  • About-ecological-transition-decarbonization-and-HVAC-systems

    A modular chiller system solution for an office building

  • About-ecological-transition-decarbonization-and-HVAC-systems

    District cooling solution for a whole new neighborhood in Milan

  • About-ecological-transition-decarbonization-and-HVAC-systems

    Providing efficient solutions within a refurbishment project involving a hospital

  • About-ecological-transition-decarbonization-and-HVAC-systems

    Providing schools with efficient mechanical ventilation

  • Hotel in Las Arenas, Valencia

    VRV 5 decarbonises Lincoln University

    The University of Lincoln is setting new standards in sustainable building management with the installation of a new R32-based VRV5 Heat Recovery heat pump, underlining the university’s commitment to environmental improvement and a significant move towards its net zero targets.
  • Hotel in Las Arenas, Valencia

    Supplying a temperature control solution for a railway control system

    Daikin has recently supplied a total solution to maintain temperature in the train switching system control room of a French intercity high-speed rail service.
  • Hotel in Las Arenas, Valencia

    Supplying a complete HVAC system for an office building

    Daikin has recently supplied a complete solution for an office building of a Dutch company in the flower import/export business.
  • Heilig Hart Leuven

    Maximizing Uptime and Energy Saving by Using Remote Monitoring ​at Heilig Hart Regional Hospital

    Heilig Hart Regional Hospital purchased Daikin air-cooled chillers since 2020. The units are positioned on the roof of its central building, for cooling the hospital and its critical equipment. These chillers are covered with a service contract, of which one chiller has an all-inclusive extended warranty contract.
  • Romianian school with Daikin ventilation and AP system

    School Indoor Air Quality Trials Romania

    Top of the class: Daikin commercial ventilation and air purification systems demonstrate the benefits of improved air quality on student performance.
  • Hotel in Las Arenas, Valencia

    VRV 5 decarbonises Lincoln University

    The University of Lincoln is setting new standards in sustainable building management with the installation of a new R32-based VRV5 Heat Recovery heat pump, underlining the university’s commitment to environmental improvement and a significant move towards its net zero targets.
  • Hotel in Las Arenas, Valencia

    Caleido Tower, Madrid

    The Caleido Tower, also known as the Fifth Tower, is situated in the business district of Paseo de la Castellana in Madrid.
  • Heilig Hart Leuven

    Maximizing system continuity via reliable remote monitoring services at NPF Nuova Presso Fondal SpA

    NPF Nuova Presso Fondal purchased Daikin air-cooled chillers in 2020. The units are used for cooling and maintaining the temperature of mould cooling water in aluminium die-casting activities.
  • AHT Rottenmann

    A decarbonization project for a gas boiler replacement at the factory of AHT Rottenmann

    AHT Cooling Systems is the leading provider of plug-in, environmentally friendly deep-freeze systems and a perfect partner for food retailers and food manufacturers. For their factory in Rottenmann, Daikin realized an industrial heat pump project to replace gas boiler heating and support AHT’s ambition to reduce the carbon footprint of their facilities.
  • Venice museum

    Daikin Elevates Climate Control at Iconic Venice Museum

    In a bid to enhance both comfort and sustainability, Daikin, a global leader in heating, ventilation, and air conditioning (HVAC) solutions, has recently unveiled a pioneering initiative at a renowned museum nestled in the heart of Venice, Italy. Four cutting-edge EWWQ-G heat pumps have been seamlessly integrated to cater to the museum's diverse heating and cooling requirements.
  • Venice museum

    A new chiller replacement provides energy efficiency for residential buildings

    Discover how Daikin's EWAD-M chillers are revolutionizing cooling in Abu Dhabi's residential landscape. With unparalleled energy efficiency and reliability, these state-of-the-art units exceed cooling demands, ushering in a new era of sustainability and profitability.
  • Venice museum

    Providing public buildings with IAQ

    In a bold move towards enhancing indoor air quality and operational efficiency, Daikin has rolled out a mechanical ventilation solution equipped with heat recovery capabilities and specialized filters.
  • Venice museum

    Basildon Hospital

    Hospital’s rapid chiller change beats effects of climate change
  • Venice museum

    Perfumiarnia

    Perfumiarnia, a unique project of high-class apartment buildings in a former perfume factory in Poznań, Poland, decided to equip their apartments with the mini VRV5 air to air heat pump system with R32 refrigerant.
  • Garitage Park

    Garitage Park

    Big, bigger, Garitage Park: This 360° HVAC solution delivers the perfect climate for work, life, and play.
  • The benefits of using heat recovery mechanical ventilation in retail applications

    A case study of Daikin in Belgium: discover energy savings, improved air quality, and sustainability benefits of heat recovery ventilation in retail.
  • How Daikin Fan Coil units contribute to Green Building Projects

    Learn how Daikin Fan Coil Units enhance energy efficiency and sustainability, supporting green building projects with BREEAM and LEED certifications.
  • Complete Daikin HVAC solution for modern BMW garage in Aalst

    BMW and Daikin - two major brands that prioritise sustainability, comfort and experience. In the middle of April, the impressive Meerschman BMW garage opened in Erembodegem, Aalst. Designed by Willy Naessens Industriebouw, the modern infrastructure is immediately eye-catching. Not just wonderful to look at, the building is also ecological and future-proof, designed in a way to prioritise the customer experience.
  • A combination of air handling units and VRVs for Daikin's 30,600m² state-of-the-art facility

    Discover how Daikin’s EDC Ghent integrates VRV & AHU systems for energy-efficient heating & cooling in a 30,600m² research hub.
  • Why air-sourced heat pumps are a smart choice for hotels

    Explore how Daikin’s EWYE-CZ heat pump delivers reliable heating, cooling, and hot water for hotels: efficient, compact, and easy to integrate.
  • Prologis Valencia warehouse gets fast, scalable HVAC solution from Daikin

    Discover how Daikin's expertise in commercial HVAC technology helped Prologis prevent heat-related shutdowns with a fast, energy-efficient HVAC solution for its 20,000 m² warehouse in Valencia
  • The new Research and Development Center of Daikin Europe

    Daikin’s new European R&D Center in Ghent stands as a global innovation hub for sustainable heating and cooling. The €140 million facility drives next-generation heat pump technology, doubles testing capacity, and strengthens collaboration with Ghent University to advance the energy transition across Europe, the Middle East, and Africa.
  • Daikin EWWH-J-SS powers Beform's industrial growth in Norway

    Daikin’s EWWH-J-SS heat pumps help Beform Norge achieve stable process cooling, lower energy use and future-ready, sustainable industrial operations.
  • Daikin delivers Europe‘s first fully-integrated CO₂ solution for food retail at Dennree GmbH​

    The new Denns BioMarkt in Wiesbaden marks a first for European food retail: commercial refrigeration, heating and air conditioning all running on a single natural refrigerant – CO₂ (R-744).​
  • A Shared Vision for the Future: Emondt Multiclima and Daikin partner to install Netherlands’ first CO₂ VRV​

    When it came to updating its own offices, Emondt turned to Daikin to explore the options to make a leap in future-proof​ HVAC design.​