Skip to main content

Hoteles Santos • Las Arenas

Valencia, Spain

Lowering operation costs while staying operational

The existing HVAC-R system was installed in 2007. After 13 years, a system update was preferred to enhance efficiency. The latest technological advancements of new Daikin systems ensure a future-proof and energy-saving operation while keeping a top level comfort. Even the existing indoor units and piping could be reused, so there was no need to close the hotel for a renovation.

With this system update an efficiency increase of 30 % was achieved right from the start. Compared with a complete new installation this was reached with a much lower investment. The fast and gradual installation reduced business disturbances to a minimum and allowed to keep the hotel open during the whole installation process.

Solution at a glance

  • 88 outdoor units
  • 458 indoor units
  • Central control with Intelligent touch Manager
  • Installation and maintenance monitoring with Daikin Cloud Service

Learn more

Our other cases

  • A Shared Vision for the Future: Emondt Multiclima and Daikin partner to install Netherlands’ first CO₂ VRV​

    When it came to updating its own offices, Emondt turned to Daikin to explore the options to make a leap in future-proof​ HVAC design.​
  • Daikin delivers Europe‘s first fully-integrated CO₂ solution for food retail at Dennree GmbH​

    The new Denns BioMarkt in Wiesbaden marks a first for European food retail: commercial refrigeration, heating and air conditioning all running on a single natural refrigerant – CO₂ (R-744).​
  • Daikin EWWH-J-SS powers Beform's industrial growth in Norway

    Daikin’s EWWH-J-SS heat pumps help Beform Norge achieve stable process cooling, lower energy use and future-ready, sustainable industrial operations.
  • The new Research and Development Center of Daikin Europe

    Daikin’s new European R&D Center in Ghent stands as a global innovation hub for sustainable heating and cooling. The €140 million facility drives next-generation heat pump technology, doubles testing capacity, and strengthens collaboration with Ghent University to advance the energy transition across Europe, the Middle East, and Africa.
  • Prologis Valencia warehouse gets fast, scalable HVAC solution from Daikin

    Discover how Daikin's expertise in commercial HVAC technology helped Prologis prevent heat-related shutdowns with a fast, energy-efficient HVAC solution for its 20,000 m² warehouse in Valencia
  • Why air-sourced heat pumps are a smart choice for hotels

    Explore how Daikin’s EWYE-CZ heat pump delivers reliable heating, cooling, and hot water for hotels: efficient, compact, and easy to integrate.
  • A combination of air handling units and VRVs for Daikin's 30,600m² state-of-the-art facility

    Discover how Daikin’s EDC Ghent integrates VRV & AHU systems for energy-efficient heating & cooling in a 30,600m² research hub.