Skip to main content

Daikin EWWH-J-SS Powers Beform's Industrial Growth in Norway

Project overview

BEFORM NORGE AS, a leading plastics manufacturer in Norway, is investing to reinforce Scandinavian industrial production. To support their ambitions for resilient, efficient, and sustainable operations, they partnered with Daikin to install two high-performance EWWH-J-SS water-to-water heat pump units – dedicated to precise industrial process cooling and heating.

 

ShapeProject challenge: Beform required a solution that would:

✔ Ensure stable temperature control for sensitive production processes 
✔ Reduce energy consumption and long-term running costs 
✔ Provide future-proof technology aligned with low-GWP refrigerant regulations 
✔ Deliver long-term reliability for a growing industrial facility

 

Daikin solution: two EWWH-J-SS water-to-water heat pumps

Daikin supplied and commissioned two EWWH-J-SS units, equipped with single-screw compressor technology. These units deliver high efficiency in both cooling and heating modes, making them ideal for year-round industrial process control.

Key features of the solution

  • In-house developed single-screw compressor 
  • Direct-expansion plate heat exchanger (evaporator) 
  • Shell-and-tube condenser for reliable heat exchange 
  • Compact design with a single refrigerant circuit for easy installation 
  • Compatible with low-GWP refrigerants for future compliance

This system ensures maximum heat transfer, minimal pressure drop, and dependable performance — even under fluctuating industrial loads.

 

Results and benefits

  • Stable process performance thanks to precise temperature control 
  • Lower energy consumption and reduced operational costs 
  • Future-ready and compliant with refrigerant regulation and sustainability goals 
  • Long-term reliability using robust industrial-grade components 
  • Modular scalability to support future production expansion

About Beform Norge AS

Beform is a leading plastics manufacturer with a strong focus on sustainability, quality, and innovation. Their ambition is to strengthen Scandinavian industrial production and be a trusted, forward-looking partner.

“We deliver tailor-made solutions of the highest quality and build trust through reliability and strong collaboration — both today and in the future.”

About the Installer: Ringerike Kjøl og Frys

A trusted local provider of cooling and freezing solutions, supporting both residential and commercial sectors. They offer complete support from planning and system design to final commissioning. 

Related articles

Find more information

Take a tour in our virtual showroom

Need help?

Find more information

Corporate Information

Need help?

Find more information

Corporate Information

Need help?

Looking for a new challenge?

Need help?