The new Small Inverter Chiller providing heating for a public swimming pool
Daikin has recently supplied two new Small Inverter Chillers with R-32 (in the heating version) as a replacement for the old heat pumps at the Public Swimming Pool of Vila Pouca de Aguiar in Portugal. The new units will complete the pre-existing HVAC system.
Products Installed:
- 2x EWYT-CZ
- 2x EWYQ-B
Total heating capacity: 280 kW
Why need for new units?
The main goal of this project was replacing two air-cooled heat pumps which were unreliable and did not properly meet the needs of the facility, leaving the client with insufficient heating issues.
The requirement was to replace the old heat pumps with new units that are reliable, efficient and environmentally friendly.
More about the product installed
The new Small Inverter Chiller series stands out for providing the best efficiency levels in the market, both in cooling and heating mode, and the lowest direct and indirect CO2 emission levels. That makes the new Small Inverter Chiller a great environmentally-friendly choice, also thanks to the use of R-32, which is known for being a low GWP and a sustainable refrigerant.
Read more here about the new Small Inverter Chiller
Besides the series being efficient and environmentally friendly, its features such as a reduced carbon footprint, silent performance and advanced connectivity were also greatly appreciated. This made the new range a perfect choice for the project.
When it comes to reliability, Daikin is the pioneer and expert in developing R-32 technology.
In 2018, Daikin was an early innovator and made history by introducing the first R-32 refrigerant chillers, followed by free-cooling scroll units the same year, and the R-32 Heat Pump in 2020.
Today, Daikin has the highest number of R-32 installations in the world, a true testimony to the experience, the knowledge, the quality and the reliability of its R-32 products.
Read more here about our expertise in R-32 technology development