AHT Cooling Systems is the leading provider of plug-in, environmentally friendly deep-freeze systems and a perfect partner for food retailers and food manufacturers. For their factory in Rottenmann, Daikin realized an industrial heat pump project to replace gas boiler heating and support AHT’s ambition to reduce the carbon footprint of their facilities.
About the project
For this project Daikin had to come up with an efficient, smart, and sustainable heat pump systems solution, able to provide a sustainable, flexible, energy saving and reliable solution to cover AHT’s year-round heating demands. The comprehensive Daikin industrial heat pump portfolio met all of the customer’s requirements, including full compatibility with the existing photovoltaic system as an energy source.
The solutions consisted of a heat pump cascade with a totally installed heating capacity of 1,200 kW for heating of the production facility, the office building and for domestic hot water supply. Additionally, a further extension of a heat pump installation of 500 kW is planned to be added in the future.
More about the solution supplied
The project scope included the delivery and assembling of all Daikin heat pumps, supervision during the installation, commissioning, testing and functional checks and a contract for maintenance.
After taking all the requirements into consideration, Daikin designed a solution consisting of four air-cooled Daikin heat pumps with R-32 refrigerant as energy source for two water-to-water heat pumps EWWH-VZ featuring R-1234ze refrigerant to ensure year-round heating of AHT facilities and deliver a hot water production of up to +73°C. An energy loop with temperature levels of 15°C to 20°C ensures maximum efficiency of the heating system.
Discover Daikin R-32 heat pump
Are you working on a similar project and want to know more about Daikin solutions for the retail sector? Then, get in touch with your local Daikin representative.
About Daikin Europe N.V.
Daikin Europe N.V. is a subsidiary of the global group Daikin Industries, and the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC&R) technology in Europe, Middle East and Africa. Daikin designs, manufactures, and brings to market a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial and industrial purposes. To date, Daikin Europe has over 13,700 employees across more than 57 consolidated subsidiaries. It has 14 manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. The headquarters of the Daikin Europe group are in Ostend, Belgium. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Daikin Industries was founded in 1924, in Osaka, Japan. The global group employs over 96,000 people worldwide and is the market leader for heat pump and air conditioning systems and air filtration. It is the world’s only manufacturer that develops and manufactures heating, ventilation, air conditioning and refrigeration equipment, as well as refrigerants in-house. The company achieved € 28.2 billion sales turnover in fiscal year 2022 (1 April 2022 – 31 March 2023).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462321 Mail: kakinaga.d@bxl.daikineurope.com