Skip to main content

Daikin expands its AI data center portfolio with the new Coolant Distribution Unit

An integrated solution for high-density rack liquid cooling, combining coolant distribution and advanced control of the entire Data Hall

Ariccia, November 02, 2026 – The rapid growth of Artificial Intelligence and Machine Learning applications is reshaping data center infrastructure requirements, driving higher IT power densities and creating new thermal management challenges. To address these evolving needs, Daikin introduces its new Coolant Distribution Unit (CDU), available for order starting November 1, 2027. Specifically developed to support high-density AI applications, the new CDU is designed to enable thermal energy transfer between the Facility Water System (FWS) and the Technology Cooling System (TCS), supporting stable and reliable operating conditions in environments characterized by high thermal loads.

Product features

The new CDU range has been designed to provide a high degree of application flexibility, addressing the requirements of a wide variety of data center projects, both in new installations and retrofit applications. The units offer capacities ranging from 400 kilowatts to 2.5 megawatts per CDU and can be configured to support different TCS circuit management strategies. Through proprietary control logic, up to ten units can operate in parallel as a single integrated system, providing centralized control of circuit temperature and pressure. For larger-scale applications, the range also includes preassembled and engineered skid solutions featuring multiple CDUs integrated and configured for parallel operation. This approach can help simplify installation and commissioning activities while reducing on-site integration requirements. In addition, the use of standardized configurations may support project execution by facilitating procurement and coordination activities throughout the implementation process.

Reliability, serviceability and operational control

The new CDU has been designed to support the high availability requirements typically associated with modern data center environments. The system architecture incorporates features intended to enhance system resilience, including redundant pumps, duplicated pressure and temperature sensors, an integrated leak detection system, advanced alarm management functions and options supporting continuity of electrical supply. The hydraulic circuit is manufactured entirely from AISI 316L stainless steel and incorporates grooved mechanical couplings throughout, eliminating the need for welded joints. This design has been selected to provide corrosion resistance and to facilitate installation and maintenance activities throughout the equipment lifecycle. Particular attention has also been dedicated to serviceability. All units within the range are designed for front-side access only, reducing service clearance requirements. In addition, pumps can be removed using dedicated sliding rails designed to facilitate maintenance operations and support faster component replacement.

Daikin controller and group control logic

The CDU is equipped with a controller developed by Daikin for the coordinated management of multiple units operating within the same system. Through proprietary control logic, multiple CDUs can operate as an integrated solution, enabling centralized management of key operating parameters. To address the requirements of AI-oriented data centers, where thermal loads may vary rapidly, the CDU combines variable-speed pumps, high-accuracy flow, pressure and temperature measurements, and dynamic adjustment of TCS operating parameters. This control approach is designed to support stable operating conditions across a wide range of load profiles. A key element of the solution is a modulating valve dedicated to the FWS primary circuit, featuring an equal-percentage control characteristic and a high-speed actuator. The valve is designed to regulate thermal energy exchange between the FWS and TCS circuits and to support control of the TCS outlet temperature according to the configured operating parameters.

iDCM evolves from chilled water plant control to full data hall management

With the introduction of the new CDU, Daikin further expands its data center offering through the evolution of the iDCM (Intelligent Data Center Manager) platform, extending its scope beyond traditional chilled water plant control. The platform is designed to monitor and coordinate a broader range of equipment deployed within the Data Hall, including CDUs, CRAHs, AHUs and Fan Wall systems, providing operators with a centralized view of cooling infrastructure operating conditions. Through a single interface, iDCM enables visualization of temperatures, unit status and alarms in real time, while also providing access to selected operating parameters and supporting diagnostic and troubleshooting activities. The platform can also be integrated with existing Building Management Systems (BMS), facilitating coordinated management of the cooling infrastructure within the broader facility control environment.

About Daikin

Daikin Europe N.V.

The Daikin Europe Group is a leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, the Middle East, and North Africa. It serves a diverse customer base across the region by designing, manufacturing, and marketing a wide range of products, maintenance services, and turnkey solutions for residential, commercial, and industrial applications. The company employs more than 14,200 people through 57 subsidiaries and operates 15 manufacturing sites in Europe (12), Turkey (1) and the Middle East (2). Daikin’s refrigeration products are available under the Daikin, Tewis, Zanotti, Hubbard, and AHT brands. Headquartered in Ostend, Belgium, for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.

About Daikin Industries Ltd.

Daikin Industries is a global leader in heat pump, air conditioning, and air filtration technology. The company employs more than 104,000 people worldwide. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 innovative companies by Clarivate (UK) and LexisNexis (USA), recognised for its leadership in technology research and intellectual property patents. For its fiscal year 2025 (1 April 2025 – 31 March 2026), Daikin reported record-high sales of 5.02 trillion yen (28.66 billion euros at reporting rate). 

Read more on www.daikin.eu and www.daikin.com. 

Media Contacts Daikin Europe N.V.

Sofie Sap – T.:  +32 472 580 482 Mail: sap.s@daikineurope.com

Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com

Related articles

Find more information

Take a tour in our virtual showroom

Need help?

Find more information

Corporate Information

Need help?

Find more information

Corporate Information

Need help?

Looking for a new challenge?

Need help?