Caleppio di Settala, 16 November 2026 – Daikin announces the launch of Daikin Vertical Water and the new Daikin Space Cooler & Heater range, available in both DX and Hydronic versions. Available from November 2026, these new solutions expand Daikin’s large-space HVAC portfolio, offering greater design flexibility for warehouses, logistics centres, manufacturing facilities, gyms and sports venues. With direct-expansion and hydronic options, the ranges are designed to deliver even heating and cooling for new-build and retrofit projects.
Two technologies for different system requirements
The new ranges are available in both DX and Hydronic versions, allowing the solution to be tailored to each building's specific characteristics. DX versions use refrigerant as the distribution medium and can be combined with Daikin VRV 5 systems or ERA condensing units. This configuration is suitable for new buildings, extensions to existing systems, or applications where no hydronic network is available. Hydronic versions use hot or chilled water distributed through networks connected to chillers or heat pumps. This solution is particularly suitable for commercial and industrial buildings that already have centralised hydronic infrastructure, as well as refurbishment projects where the existing system can be leveraged while minimising structural modifications, and can be retained, helping to limit structural modifications.
Daikin Vertical: the floor-standing solution designed for retrofit projects
Daikin Vertical has been designed for applications where ceiling installation is impractical or complex. Thanks to its floor-standing configuration, the unit can be integrated into existing buildings, simplifying installation and limiting disruption.
Available in both DX and Hydronic versions, Daikin Vertical delivers a nominal airflow rate of 4,000 m³/h and is designed to distribute conditioned air evenly across large spaces. The ready-to-connect configuration can further simplify installation: both the control panel and coil connections can be positioned on either the right-hand or left-hand side of the unit.
Daikin Space Cooler & Heater: heating and cooling without occupying floor space
Daikin Space Cooler & Heater provides heating and cooling for large industrial and commercial spaces without using floor space. Thanks to its wall- or ceiling-mounted installation, it is ideally suited for warehouses, production facilities, and logistics centres. Featuring a nominal airflow rate of 4,000 m³/h, the unit combines high air delivery with adjustable nozzles to direct airflow towards the required areas and support even temperature distribution.
Simplified installation and maintenance
Both ranges are designed to simplify installation, operation and maintenance. The ductless design can reduce system complexity and commissioning time, helping to limit disruption in industrial and logistics facilities. The units also feature dedicated filtration systems designed to filter the air and help protect internal components over time.
Made in Italy and available from stock
Daikin Vertical and Daikin Space Cooler & Heater are designed and manufactured at the Daikin Applied Europe facility in Caleppio di Settala (Milan). Bringing design and production together on-site allows Daikin to maintain close oversight of quality and performance throughout the manufacturing process.
Both ranges will also be available from stock in a wide range of configurations, which can shorten lead times and support faster project delivery, particularly in retrofit, replacement, and system expansion applications.
About Daikin
Daikin Europe N.V.
The Daikin Europe Group is a leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, the Middle East, and North Africa. It serves a diverse customer base across the region by designing, manufacturing, and marketing a wide range of products, maintenance services, and turnkey solutions for residential, commercial, and industrial applications. The company employs more than 14,200 people through 57 subsidiaries and operates 15 manufacturing sites in Europe (12), Turkey (1) and the Middle East (2). Daikin’s refrigeration products are available under the Daikin, Tewis, Zanotti, Hubbard, and AHT brands. Headquartered in Ostend, Belgium, for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.
About Daikin Industries Ltd.
Daikin Industries is a global leader in heat pump, air conditioning, and air filtration technology. The company employs more than 104,000 people worldwide. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 innovative companies by Clarivate (UK) and LexisNexis (USA), recognised for its leadership in technology research and intellectual property patents. For its fiscal year 2025 (1 April 2025 – 31 March 2026), Daikin reported record-high sales of 5.02 trillion yen (28.66 billion euros at reporting rate).
Read more on www.daikin.eu and www.daikin.com.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com