Skip to main content

Claerhout Communication House Office

Ghent, Belgium

bg-image

Claerhout Communication House is a full service advertising and communications agency. When opening their new office building, which provides office space for 45 employees and a conference room for 150 guests, flexibility was a highly important requirement in the design. It has to be easy to subdivide the large open spaces into smaller rooms. And it has to be easy to change the layout in function of future assignments and activities of the employees.

The main goals that were to be achieved were:

  • 30% less running costs
  • 50% less CO2 emissions
  • A healthy and comfortable working environment
  • A lean construction principle.

“Daikin experts give answers to our questions and provide the appropriate solution: refrigeration for the kitchen, cooling for the server room, virtually free hot water for the caretaker’s apartment and units for spaces without raised floors or a false ceiling. A completely integrated system with Daikin as the only supplier and point of contact.”

- Pieter Claerhout, CEO and owner of Claerhout Communication House

Open landscape office

Our employees work in an open landscape office. To efficiently be able to keep the temperature at a constant and comfortable level we opted for a Daikin heat recovery system.

Whenever the offices at the southern side get too warm the excess warmth is recovered for providing additional heating. 

Claerhout heat recovery

Mix of different VRV units

bg-image

It is possible to subdivide the large open spaces into smaller rooms. This is why we opted for a mix of different VRV units: VRV heat recovery systems that ensure the comfort of the staff in the small individual offices where only a single person is working while cooling is needed in another room for a team meeting. We installed VRV heat pump systems for large meeting spaces since all of these have the same orientation.

The installation method used in this building is exceptional. Because the building owner did not want any false ceilings the entire technical infrastructure was fitted under a raised floor. Concealed units were used in this regard. The advantage of these units is that during setup the fan speed is automatically adjusted to overcome the resistance in the ducts. In that way we ensure optimal comfort and installation time is reduced.

Learn more

Our other cases

  • A high efficiency solution for a residential building

    This residential project was executed in the context of the renovation of a residential building, which had energy efficiency as a main aspect.
  • ACTION

    As a discount retailer, cost has been a major factor in the choice of HVAC systems for Action, who sought an HVAC supplier that could also give HVAC design and support and offer local coordination in each expansion country.
  • Action reclaimed refrigerant allocation

    Action intensifies its partnership with Daikin for this new ground breaking project: reclaiming refrigerant from its refurbished stores and reusing it.
  • Biocoop

    Daikin completes the installation and commissioning of the first transcritical CO2 refrigeration solution on the French market at a meat processing laboratory in the Dordogne.
  • Bringing Air Conditioning in stadiums

    A Daikin R-32 chiller has recently been installed and commissioned in a HVAC project involving a stadium in Sittard, in the Netherlands.
  • C&A

    Looking to renovate its entire HVAC system, the C&A store wanted to achieve year-round comfort in the most cost-effective and efficient way.