Brussels, 13 June 2024 – Daikin is launching the new polyvalent unit EWYS-4Z, equipped with Daikin inverter-driven, single-screw compressors. It is designed for simultaneously cooling and heating commercial and industrial applications in an efficient and reliable way. The new multipurpose unit operates with R-513A refrigerant, of which the Global Warming Potential (GWP) is 55% lower than R-134a, while maintaining the same safety classification (A1).
Reliable operation and optimal performance in variety of applications and circumstances
The Daikin EWYS-4Z polyvalent unit features highly efficient single-screw compressors with Variable Frequency Drive (VFD) and Variable Volume Ratio (VVR). Key information about the EWYS-4Z range:
Capacity range: from 400 to 800 kW in cooling and heating mode
Total Energy Efficiency Ratio (TER) up to 7.89
Operating temperatures: from -18°C to +50°C ambient temperature
Chilled water temperature range: from -8°C (with water/glycol mixture) to +20°C
Heating water temperature range: from +30°C to +60°C
As a result, EWYS-4Z can be extensively used across a variety of applications: industrial or commercial buildings, hotels or hospitals. It also ensures reliable operation and optimal performance in many distinct locations and weather conditions. A reduced noise configuration is also available, featuring noise attenuation achieved through lower fan speeds and a specially designed soundproof compressor cabinet. Enhanced insulation on refrigerant pipes and special connections at the compressor's suction significantly reduce vibration transmission.
How this multipurpose unit simultaneously meets cooling and heating requirements
The EWYS-4Z is equipped with two Shell&Tube heat exchangers on the waterside: one always operates as an evaporator (cold heat exchanger) and the other as a condenser (hot heat exchanger). Copper-aluminium (Cu/Al) fin and tube coils are used to dissipate excess cooling or heating energy.
As a result of this design, the Daikin polyvalent unit can simultaneously meet cooling and heating requirements by following two setpoints simultaneously all year round, adapting to changing climatic conditions. Unlike reversible heat pumps, it does not require seasonal changeover and can control the two refrigerant circuits independently, based on actual cooling and heating demand.
Ten reasons to choose Daikin’s multipurpose unit
Multipurpose units are preferred for applications requiring simultaneous heating and cooling. Therefore, the main challenges when to choose these units relate to the following aspects:
How efficient and reliable operation is guaranteed
To what extent they can be integrated in a larger HVAC system
How to keep their reliability and performance over time
Daikin’s new multipurpose unit EWYS-4Z offers 10 compelling advantages, outlined below:
Efficient operation to limit running costs
1. VFD regulation combined with VVR control
The EWYS-4Z range provides chilled and hot water operating in both air-to-water and water-to-water all year round. The VFD modulates unit capacity efficiently at part load, while VVR adjusts compressor operations to match any conditions, minimizing energy losses.
2. No starting current
No current spikes at start-up. The starting current is always lower than the current absorbed in the maximum operating conditions (FLA).
3. High power factor
EWYS-4Z maintains a displacement power factor always greater than 0.95, avoiding power factor penalties and reducing electrical losses in cables and transformers.
4. Quick comfort conditions and low water content required
The ability to vary the output power in direct relation to the cooling and heating requirements of the system, allows to reach the set-point conditions very quickly. The switch between the different operating modes occurs in less than one minute allowing it to operate properly with the same amount of water as in the loop of a cooling-only inverter chiller.
Outstanding reliability
Reliable operation is ensured considering both product and control features at the same time.
5. EWYS-4Z is designed with two separate and independent refrigerant circuits ensuring maximum safety and ease of maintenance.
6. Daikin refrigerant-cooled VFD technology is not affected by environmental conditions such as ambient temperature, altitude or air quality, ensuring unparalleled reliability.
7. Thanks to meticulous design and experience, Daikin single-screw compressors feature highly balanced mechanical loads. These reduce component stress, extend the life of the unit, and improve reliability. This design also minimises vibration and noise emissions. The excellent volumetric efficiency of the compressors makes them ideal for variable-speed applications. The compressor geometry is optimised for variable speed operation, even at high speeds.
8. Daikin intelligent Chiller Manager (iCM) allows control of up to 8 units within a system. It manages the sequencing and capacity of each unit to achieve the overall required capacity while minimizing energy consumption. That ensures proper sequencing and capacity management of the units without the need for an additional control panel, utilizing the unit’s software functionalities. This approach provides a highly cost-effective plant solution, prioritizing reliability over efficiency. It balances the load between units, optimizes the working conditions of the entire group and extends the life of the units in the system.
Integration of multipurpose unit in a larger HVAC system
9. Daikin intelligent Control Manager (iCM) ensures proper integration of EWYS-4Z units into a system with distinct types of units, such as:
A 4-pipe system with EWYS-4Z and a chiller with heat recovery
A 4-pipe system with EWYS-4Z and a heat pump with a changeover valve for mode-switching
In both cases, a full Daikin HVAC system can be designed. In the second case, the integration with water-to-water heat pumps (under the same system control) allows for a full decarbonization of heating even where terminals would still be radiators. A Daikin cascade system can be designed for provision of heating water up to 75 °C, considering EWYS-4Z in combination with single screw compressor’s water-sourced heat pumps, eventually also equipped with VFD, and available under various refrigerant options (R-1234ze, R-513A, R-134A).
Reliability and performance over time
10. It is key to keep HVAC equipment under proper conditions, to fulfil HVAC plant targets and related maintenance costs.
EWYS-4Z is equipped with Daikin on Site, a cloud-based remote monitoring system that provides 24/7 real-time data, ensuring the proper functionality of cooling and heating plants. This innovative tool for HVAC systems offers not only remote monitoring, but also periodic reports for in-depth plant analysis, energy analysis and intelligent maintenance.
Daikin on Site delivers a unique level of detail, offering a continuously evolving service that enables plant owners to take preventive measures and avoid additional costs associated with breakdowns and downtime. Facility managers can easily identify problems and find the right solutions whenever an alarm occurs. The platform allows for real-time evaluation of parameters, making it possible to adjust settings and intervene remotely when needed.
With Daikin on Site, users have complete access to the unit controller through the cloud. The unit is equipped with a modem and a mobile phone card, providing an autonomous internet connection.
About Daikin
About Daikin Europe N.V.
Daikin Europe N.V. is a subsidiary of the global group Daikin Industries, and the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC&R) technology in Europe, Middle East and Africa. Daikin designs, manufactures, and brings to market a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial, and industrial purposes. To date Daikin Europe has over 13,700 employees across more than 57 consolidated subsidiaries. It has 14 manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. The headquarters of the Daikin Europe group are in Ostend, Belgium. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Daikin Industries was founded in 1924, in Osaka, Japan and is celebrating its 100th anniversary this year. The global group employs over 96,000 people worldwide and is the market leader for heat pump and air conditioning systems, as well as air filtration. It is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning and refrigeration equipment, as well as refrigerants in-house. The company achieved € 28.2 billion sales turnover in fiscal year 2022 (1 April 2022 – 31 March 2023).
Read more on www.daikin.eu and www.daikin.com.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462321 Mail: kakinaga.d@bxl.daikineurope.com