New from Daikin comes the latest innovation in heat pump technology for the home. The high efficiency Multi + heat pump combines room cooling and heating with domestic hot water in a single energy-saving system.
A perfect match
Good for homeowners and the environment, the Multi+ heat pump uses state of-the-art technology to create a comfortable home all year round, while always ensuring a plentiful supply of hot water. Drawing on the external ambient air, Multi + saves energy and keeps running costs down.
User-friendly controls with app-controlled access allows settings to be adjusted to fit around homeowners’ individual needs.
Requiring minimal space, the Multi + is quick and easy to install, making it an ideal replacement option for Domestic Hot Water (DHW) systems where air conditioning is also a requirement.
Custom design at an affordable price
Offered with a choice of domestic hot water storage capacities of either 90 liters or 120 liters, the Multi+ heat pump can be connected to two or three air conditioners*, allowing the system to be extended according to household needs. A wide range of indoor units, with several award-winning designs, are available to meet aesthetic and room space requirements, including wall-mounted, floor-standing and concealed ceiling models.
Engineered for performance and choice
Programmable settings to allow users to schedule system operation around their own lifestyle without compromising on energy savings or home comfort.
DHW heating can be scheduled to run during the day when nobody’s home or early in the morning. The DHW tank is programmed to heat up the water to a preset value. Set point temperatures may be adjusted to either ECO (50˚C) or COMFORT (60˚C) according to personal choice.
The system also features a weather-dependent setting, where the water temperature is determined automatically by the external temperature. If the outdoor temperature drops or rises, the unit compensates instantly without requiring user adjustment, which prevents sudden changes in the water temperature at tap points.
The Multi + allows homeowners to set priorities for air conditioning and DHW depending on preference. Space heating and DHW heating can be set to operate simultaneously for maximum comfort and efficiency. Where cooling is required, the previously heated DHW is used, providing cooling and hot water at the same time. The A/C priority setting ensures air conditioning stays active for maximum comfort. Additional hot water will then be heated with the electric booster heater as required. Switching to DHW priority deactivates the air conditioning while reheating the water with the heat pump, saving on energy bills. Once the DHW operation is complete, the outdoor unit can be switched back to A/C operation.
The Multi + heat pump has been engineered to provide the highest standards of reliability and efficiency, incorporating several important innovative design features including an innovative fan design, with specially shaped fan blades that significantly reduce sound emissions and lower power consumption, concealed behind an elegant front grille. Additionally, its powerful high-efficiency swing compressor continuously adjusts the system’s cooling and heating output to maintain desired room temperatures.
Control in your hands
The Multi + heat pump’s user-friendly controls let homeowners configure the system the way they want it. The tank control panel, with an intuitive full-text display, makes it easy to optimise temperature and function settings. Daikin’s Onecta app, compatible with Amazon Alexa and Google Assistant, allows scheduling, control and monitoring of individual air conditioning units and the domestic hot water system from anywhere, at home or away.
Forward thinking
Daikin are worldwide market leaders in delivering heat pump solutions for the home.
Daikin’s decarbonization strategy, aimed at achieving Net Zero CO2 emissions by 2050, combines the use of low GWP refrigeration with the development of advanced technologies to deliver super-efficient systems while minimising environmental footprint.
Available from 1st April, the Multi+ is a clever idea for temperature regulation for homeowners wanting to conserve resources and save energy costs without compromising on home comfort.
For more information visit: Multiplus
*Note: FBA60-71 allows connection to a single unit only.
Every year in May we will provide an update of this text.
Press release
-
MULTI PLUS_DEUEN22-026_PRESS RELEASE_ENGLISHZIP | 145.31MB
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com