Brussels, 24 January 2024 – Daikin has announced the release of the new FWF-D 2 x 2 Fancoil ceiling-mounted cassette, incorporating new open communication protocols that allow combination with other commercially available controllers for greater flexibility and specification choice. In addition, the new unit features a range of other enhancements designed to improve energy efficiency and simplicity of installation.
Extended capabilities
Based on the BLDC fan motor, the FWF-D Fancoil unit delivers precise operational control with a four-way air discharge for maximum airflow and offers a cooling capacity from two to five kW. The open protocol enables easy integration of third-party controllers.
Energy consumption has been reduced thanks to the FWF-D DC fan motor and drain pump.
Available as a choice of two- or four-pipe configurations, the new FWF-D cassette comes with options for two- or three-way on/off valves, available as option or fitted on the unit. Thermal insulation as standard accessory is designed to fit the shape of the valve for simpler fitting.
Low-sound performance make the FWF-D an ideal solution for working environments and shared spaces. Supplied as standard with an 835mm lift, the drain pump increases flexibility while reducing installation times.
Space-saving and elegant
Carrying through the high design standards that have earned Daikin global recognition, the new FWF-D Fancoil cassette unit fits into a standard 600 by 600mm standard architectural module.
Cassettes are available with a standard BYFQ60B3 air diffusion panel or alternatively as a fully flat decorative panel (requires additional adaptor) in a white (BYFQ60CW) or a silver/white colour (BYFQ60CS) combination for maximum concealment and style.
The FWF-D fan coil unit provides heating and cooling to create a comfortable environment for commercial spaces including offices, hotels and retail use.
The FWF-D Fancoil cassette is available to order now. For more information visit https://www.daikin.eu/en_us/products/product.html/FWF-D.html
Copyright pictures: Daikin Europe
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 13,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 96,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning and refrigeration equipment, as well as the refrigerants in-house. The company achieved € 28.2 billion sales turnover in financial year 2022.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 | Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 | Mail: kakinaga.d@bxl.daikineurope.com
Media Contact for product inquiries Daikin Europe N.V.
Kevin Viader – T.: + +32 (0)471 77 50 38 | Mail: viader.k@bxl.daikineurope.com