Daikin has announced the launch of the new Modular T series, the latest addition to the Daikin portfolio of Air Handling Units (AHU’s).
The fully optimised design of the compact Modular T, incorporating high-quality components and the latest technology, delivers a long working life and a high level of efficiency, ensuring exceptional indoor air quality
Creating a healthier environment
Every day we spend more than 90% of the time in an indoor environment but we seldom ask ourselves “How good is the air I breathe? Could it be dangerous for my health?”
All environments contain airborne pathogens, VOCs, CO2 and particulate matter. The concentration of these contaminants could potentially pose a threat to the health of building occupants.
Daikin’s Modular T AHU filters outside air to remove external pollutants prior to supply and simultaneously extracts inside air, decreasing the concentration of indoor pollutants to ensure a constant supply of healthy fresh air.
Advanced features combine to provide an innovative solution
Available in five different sizes, with an air flow range from 200 m3/h up to more than 4000 m3/h, the Daikin Modular T offers an exceptional solution for diverse applications including schools, offices, gyms, shops.
- Air purity is guaranteed, with three separate stages of filtration ensuring a safe and healthy environment.
- Plug and play connection, together with the DX Coil enables combination with VRV or ERQ condensing units to provide a complete fresh air solution, unique to Daikin.
- An integral mixing damper helps optimise consumption to reduce running costs.
Together with a comprehensive choice of accessories, these features make Modular T one of the most complete and compact AHU ranges on the market.
Its minimal footprint is one of the defining characteristics of the new Modular T unit. With a maximum depth of 890 mm for the largest model, installation has never been simpler. Other sizes in the range are equally compact at 790mm, while the smallest unit (size 03) is only 550mm deep. In addition, larger models are supplied in sections for fast, easy transportation and handling.
The Modular T is available in two different configurations, right and left, and can be equipped with either of the following control platforms:
Smart Controls
Daikin F1/F2 & P1/P2 protocols provide direct connectivity to the Daikin communication platform.
Pro Controls
Open control platform: The new Daikin Digital plug & play Digital controls ensure an easy and quick start-up of the unit as well as an efficient unit operation.
STANDARD
1. Control unit (controls and power)
2. Fresh air filter stage (one standard)
3. Return air filter stage
4. Return fan
5. Supply fan
6. Bypass damper for free cooling
7. High efficiency counterflow PHE
OPTIONAL
8. Double fresh air filter stage
9. Third filter stage/post-heating water coil
10. Recirculation/mixing damper
11. Main cooling/heating DX or water coil
Modular T component schematic shown below:
The new Modular T will be available from September 2022.
Every year in May we will provide an update of this text.
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com