Skip to main content

Daikin Unveils The New FWT-HTV Hi-Wall Fan Coil

Brussels, 24 February 2025 – Daikin introduces the FWT-HTV Hi-Wall fan coil unit range, a unit designed to deliver superior comfort, energy efficiency, and best-in-class indoor air quality. This next-generation unit integrates advanced filtration technology, including Flash Streamer, Gin-ION, and PM2.5 filters, ensuring purified air for any indoor space.

Optimised design for maximum performance

The FWT-HTV wall-mounted fan coil units feature a sleek, redesigned casing and built-in Modbus gateway, providing seamless integration into modern building automation systems. The new control platform offers both wired and wireless controller options, giving users greater flexibility and ease of operation. With a cooling capacity range of 2.4 to 5.2 kW, available in five sizes within a 2-pipe configuration, the FWT-HTV ensures adaptable, high-performance climate control. Its Brushless Direct Current (BLDC) fan motor and factory-fitted internal 3-way on/off valve further enhance its energy efficiency and precision.

FWT-HTV_R

What sets the FWT-HTV apart

The FWT-HTV range represents an ideal choice as it offers advanced features and technology. Designed to improve comfort, efficiency and indoor air quality, this range offers many benefits. Here are nine reasons why FWT-HTV is the best choice.

1. Ultra-efficient & whisper-quiet BLDC fan motor

The BLDC motor enables precise fan speed adjustments, including Quiet Mode for near-silent operation. In auto fan mode, the system intelligently adapts speeds from 40% to 100%, ensuring smooth airflow and consistent temperature control.

2. Integrated 3-way valve for enhanced efficiency

The 3-way on/off valve, included as standard, ensures precise water flow regulation, optimising thermal comfort and system efficiency. Its compact design makes it ideal for space-constrained environments, offering a versatile solution for various applications.

3. Advanced air purification for healthier indoor spaces

Daikin’s Flash Streamer technology actively decomposes bacteria, mould, and allergens, delivering purified air. Combined with Gin-ION and PM2.5 filters, the FWT-HTV ensures superior indoor air quality, making it ideal for homes, offices, and commercial spaces.

4. Smart building compliance with LEED & BREEAM protocols

The FWT-HTV supports sustainable building design, contributing to LEED and BREEAM certifications across multiple categories, including Indoor Environmental Quality, Energy Efficiency, and Waste Reduction.

5. Quiet & sleep modes for undisturbed comfort

Sleep Mode gradually adjusts temperatures to support natural sleep cycles, ensuring restful nights. In Quiet Mode, the fan speed and compressor frequency are reduced to minimise noise levels, creating a more comfortable environment.

6. Intelligent Fan Stop Control for energy savings

The Fan Stop Control function automatically halts the fan once the room reaches the desired temperature, preventing unnecessary airflow and improving overall efficiency.

7. Turbo mode for instant cooling

For rapid cooling, Turbo Mode boosts fan speed and compressor output to maximum capacity for 20 minutes, achieving faster temperature reduction before returning to normal settings.

8. Built-in self-diagnosis for easy maintenance

The self-diagnosis system detects faults and malfunctions, providing real-time alerts through LED indicators and error codes, which can be accessed via the wireless remote control for quick troubleshooting.

A smarter choice for modern climate control

The Daikin FWT-HTV Hi-Wall fan coil sets new industry standards by combining innovative air purification, energy-efficient operation, and smart controls. Whether for residential, commercial, or industrial applications, it delivers superior performance, reliability, and sustainability.

For more details on the new FWT-HTV range, visit Daikin’s website or contact our sales team.

About Daikin

Daikin Europe N.V. 

The Daikin Europe Group is a leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, Middle East, and Africa. Daikin Europe caters to a diverse customer base within this region by designing, manufacturing, and marketing an extensive range of products, maintenance services, and turnkey solutions tailored for residential, commercial, and industrial applications. The company employs over 13,800 employees through 59 subsidiaries and operates 15 manufacturing sites in Europe (12), Turkey (1) and the Middle East (2). Daikin’s refrigeration products are available under the Daikin, Tewis, Zanotti, Hubbard, and AHT brands. Headquartered in Ostend, Belgium, for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.

Daikin Industries Ltd.

Daikin Industries (DIL) is a global leader in heat pump, air conditioning and air filtration technology. The company employes over 98,000 employees world-wide. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 most innovative companies by Clarivate (UK) and LexisNexis (USA), recognized for its leadership in technology research and intellectual property patents. For its fiscal year 2023 Daikin reported a record sales result of € 28 billion sales (1 April 2023 – 31 March 2024).

 

Read more on  www.daikin.eu and  www.daikin.com

 

Media Contacts Daikin Europe N.V.

Sofie Sap – T.:  +32 472 580 482 Mail: sap.s@daikineurope.com

Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com

Related articles

Find more information

Take a tour in our virtual showroom

Need help?

Find more information

Corporate Information

Need help?

Find more information

Corporate Information

Need help?

Looking for a new challenge?

Need help?