Skip to main content

Daikin Expands AHU Portfolio with the New Compact R Range

Settala, 17 December 2025 – Daikin is expanding its Air Handling Units portfolio with the launch of Compact R, a new addition to the Compact series. This latest development introduces rotary heat recovery within a highly space-efficient casing, offering improved energy performance while maintaining the footprint that has made the Compact line a preferred choice in commercial applications. With side duct connections, installation-oriented improvements, and enhanced flexibility, Compact R further broadens Daikin’s AHU offering for modern buildings.

Developed with energy efficiency, adaptability and ease of installation at its core, Compact R combines thoughtful design, strong engineering and independently certified performance.

A versatile solution for modern commercial buildings

Compact R is available in seven sizes covering airflow rates from 500 to 6,000 m³/h, making it suitable for a wide range of environments such as shops, offices and educational facilities. The units are offered in right- or left-hand configurations, with side connections that simplify integration into different plant layouts.

Thanks to its compact dimensions, the unit can be installed indoors or outdoors, providing a flexible solution for both new projects and refurbishments. Its design supports efficient airflow management and contributes to improved Indoor Air Quality (IAQ) across various settings.

Flexibility through accessories and configuration

To adapt to diverse project needs, Compact R can be equipped with a broad selection of accessories, including electric heaters, heating coils for pre- or post-treatment, additional filtration stages and sound attenuators. This allows the system to be configured to meet the performance and comfort expectations of a wide variety of applications — from retail and hospitality to office buildings and schools.

Integration with Daikin technology

Compact R is fully compatible with the Daikin AHU-DX kit, creating a single integrated system that combines the AHU and condensing unit under one control platform. This minimises wiring, improves commissioning efficiency and ensures optimal performance. The main treatment coil — available as a water or DX coil — is integrated directly in the module, preserving the compact footprint.

The AHU-DX kit also supports decarbonisation efforts, enabling cooling and heating operation without gas boilers. It is compatible with R-410A and R-32, offering flexible and sustainable system design options.
Through Astra Web, Daikin’s AHU selection software, configuration is accurate and straightforward.

Compact R can also be combined with Daikin VRV R-32 systems for highly efficient heating and cooling, supported by built-in safety devices for R-32.

Efficient energy recovery

A rotary heat recovery wheel — available in condensation or sorption versions — allows Compact R to recover both sensible and latent heat. By transferring energy from the exhaust air to the incoming fresh air, the unit reduces overall energy consumption while maintaining stable indoor conditions throughout the year.

Reliable operation with reduced maintenance

The filtration system includes an ePM1 50% (F7) filter on the supply air and an ePM10 75% (M5) filter on the return air. This ensures high-quality indoor air while protecting internal components from dust accumulation. Combined with Daikin engineering and the compact layout, this results in a reliable, low-maintenance solution.

Certified performance

Compact R is Eurovent certified, ensuring full transparency and independent validation of all technical data. This provides designers, consultants and end users with confidence that the unit will perform as specified.

Fast availability and simplified installation

Compact R is produced following a Make-to-Stock (MTS) approach, ensuring short lead times. Larger sizes are delivered in two separate modules to facilitate handling in confined spaces, especially during renovations. While the unit is configured for indoor installation by default, an outdoor kit is available for full installation flexibility.

Compact R is delivered plug-and-play, with pre-configured settings to streamline installation and commissioning.

Smart control and performance monitoring

As a decentralised ventilation solution, Compact R enables zone-by-zone control and quick installation. Integration with the Daikin IEQ sensor allows monitoring of indoor air quality and enables Demand Controlled Ventilation (DCV), adjusting fan speed and ventilation rates according to real IAQ needs.

Compact R is also compatible with Daikin on Site (DoS), Daikin’s 24/7 remote monitoring platform. DoS improves system reliability, reduces downtime, and provides continuous performance insights.

The unit features Daikin’s Pro open control platform, offering full interoperability with modern Building Management Systems (BMS) and allowing technicians to fine-tune operation, monitor performance and implement tailored control strategies.

About Daikin Europe N.V.

The Daikin Europe group is the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, Middle East, and Africa. Daikin designs, manufactures, and offers customers a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial, and industrial purposes. To date, Daikin Europe has over 13,800 employees across more than 59 subsidiaries. It has 14 manufacturing sites in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. Headquartered in Ostend (Belgium) for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.

About Daikin Industries Ltd.

Daikin Industries (DIL) is a worldwide leader in heat pump, air conditioning, and air filtration technology with more than 98,000 employees. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 most innovative companies by Clarivate (UK) and LexisNexis (USA), recognized for its leadership in technology research and intellectual property patents. For its fiscal year 2023 Daikin reported a record sales result of € 28 billion sales (1 April 2023 – 31 March 2024).

Read more on www.daikin.eu and www.daikin.com.

Media Contacts Daikin Europe N.V.

Sofie Sap – T.: +32 472 580482 Mail: sap.s@daikineurope.com

Daisuke Kakinaga – T.: +32 465 462321 Mail: kakinaga.d@bxl.daikineurope.com

Related articles