Brussels, 2 March 2026 – Daikin announces the launch of its complete R-290 range, covering capacities from 17 to 2,000 kW across two complementary product families: the EWA(Y)K-CZ monobloc units (17- 85 kW), available in heat pump and cooling-only versions, and the EWYK-QZ modular heat pumps, scalable up to 2,000 kW. This comprehensive, future‑proof portfolio covers the a wide capacity range and supports the decarbonisation of residential, commercial and industrial applications - driven by the use of the natural refrigerant R‑290 (propane) with ultra‑low GWP, combined with high reliability and a safety‑driven design. While the EWYK-QZ is available for orders from 1 April, the EWA(Y)K-CZ will be available from mid-May.
Integrated safety as a design principle: the Daikin Safety Shield
The use of propane requires specific attention to safety aspects. Across the entire capacity range from 17 to 2,000 kW, Daikin therefore offers a system-wide package of design solutions for the most important functional areas of the unit, embodied in the Daikin Safety Shield.
A key requirement is an independent 230V power supply for all safety devices, provided by the customer, to ensure proper operation under all conditions – even in emergency situations or in the event of a failure of the unit’s main power supply. This ensures continuous monitoring and activation of the safety systems. If the power supply to the safety devices is not active, is interrupted, or is not correctly connected, the unit will not start and will remain in a safe standby condition.
The electrical switchbox is designed as a controlled environment. It is continuously pressurized and equipped with refrigerant leak detection systems, supported by ATEX-certified ventilation, visual and acoustic alarms that provide immediate indication in the event of any abnormal condition.
The R-290 refrigerant is factory-charged into dedicated storage tanks, increasing safety during transport and handling prior to installation. The refrigerant circuit also includes mechanical safety valves to manage potential overpressure conditions, with controlled discharge to the outside if required.
Additional safety measures allow any potential refrigerant dispersion to be detected and managed in a controlled manner, enabling the unit to shut down safely. The hydronic circuit is also protected: if a leak is detected, a shut-off valve isolates the water circuit, preventing refrigerant from spreading beyond the unit.
By applying the Daikin Safety Shield across both product ranges, Daikin ensures uniform safety standards and consistent design approach from small to large capacities.
Daikin EWA(Y)K-CZ: compact solution up to 85 kW
Daikin’s EWA(Y)K-CZ range covers the 17 – 85 kW segment with air-to-water monobloc units available in both heat pump and cooling-only configurations. The heat pump version can deliver leaving water temperatures of up to 75°C thanks to vapor injection technology, making it suitable for new installations as well as boiler replacement projects, even without changing the existing heat emitters The cooling-only version ensures a wide operating envelope with a minimum chilled water temperature down to -15°C with glycol covering from comfort to small-medium capacity process cooling applications. The units operate within an outdoor air temperature range from -20°C to +46°C, ensuring operational continuity under different climatic conditions.
The EWA(Y)K‑CZ units feature Daikin‑designed inverter‑driven scroll compressors and inverter‑equipped fans, both developed in‑house for optimal performance.. This configuration enables optimised modulation management, particularly relevant for variable load applications typical of multi-family residential buildings, hospitality and small- to medium-sized enterprises.
Daikin EWYK-QZ: modularity and part-load efficiency up to 2,000 kW
For bigger-capacity applications, the EWYK-QZ range adopts a modular architecture enabling multi-array configurations up to 2,000 kW working as a single integrated system. Modularity allows installed capacity to be adapted to actual project requirements, supporting both new developments and project’s expansions over time. Transport and installation are simplified, as the modular configuration provides increased flexibility in overall plant design.
The units are equipped as standard with inverter-driven scroll compressors and EC* brushless fans, enabling continuous capacity adjustment according to real system demand. Combined with the modular architecture, this approach ensures particularly efficient operation under part-load conditions, which are typical in modern buildings and many industrial processes. Continuous modulation reduces on/off cycling, contributing to improved seasonal efficiency and enhanced operational stability throughout all year round.
For complex installations, the control concept operates on two levels. Within a single array, a multiple unit sequencer coordinates and regulates alle base modules Multi-array configurations are supervised by the Daikin Intelligent Chiller Manager (iCM) optimising load distribution among units, managing sequencing efficiently and supporting continuity of service in high-capacity installations.
Qualified installation and traceable commissioning
Given the use of R-290 refrigerant, installation of the units is limited to qualified and authorised personnel. Commissioning activities must be registered via Daikin’s proprietary e-Care application. This will ensure traceability of start-up operations and guarantee that the system is installed and operated in line with the original design intent from trained technicians. This structured approach supports safety, operational consistency and long-term system reliability throughout the entire lifecycle.
Reference:
*EC = Electronically commutated
Copyrights pictures: Daikin
About Daikin Europe N.V.
The Daikin Europe Group is a leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, the Middle East, and Africa. Daikin Europe caters to a diverse customer base within this region by designing, manufacturing, and marketing an extensive range of products, maintenance services, and turnkey solutions tailored for residential, commercial, and industrial applications. The company employs over 13,800 employees through 58 subsidiaries and operates 15 manufacturing sites in Europe (12), Turkey (1) and the Middle East (2). Daikin’s refrigeration products are available under the Daikin, Tewis, Zanotti, Hubbard, and AHT brands. Headquartered in Ostend, Belgium, for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.
About Daikin Industries Ltd.
Daikin Industries (DIL) is a global leader in heat pump, air conditioning and air filtration technology. The company employs over 103,500 employees worldwide. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 innovative companies by Clarivate (UK) and LexisNexis (USA), recognized for its leadership in technology research and intellectual property patents. For its fiscal year 2024 Daikin reported a record sales result of € 28,98 billion sales (1 April 2024 – 31 March 2025).
Read more on www.daikin.eu and www.daikin.com.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462321 Mail: kakinaga.d@bxl.daikineurope.com