Skip to main content

Always there, embracing you with warm or cool air

True comfort you feel instantly, right down to your toes. It’s simply… there. Our air-to-water heat pumps are just like that. They heat your home, cool your spaces and provide warm water. Ready for comfort that perfectly blends into your interior?

Smart comfort, low energy use

Easy control via app or voice

All-year-round comfort in one solution

Ideal with radiators & underfloor heating

One smart system, every comfort covered

Daikin’s all-in-one heat pumps provide heating, cooling and warm water with quiet intelligence. Always there, adapting to your home and lifestyle.

  • Girl reading in a cosy room with warm floors and perfect indoor temperature

    All-in-one comfort, relax

    Warm floors in winter. Cool rooms in summer. Warm water on demand. Whether you have radiators or underfloor heating, our system adapts to both. Comfort from a single, smart solution.

  • Son embracing his mother in a welcoming hallway, symbolising the comfort, warmth, and invisible impact of clean, perfectly balanced indoor air by Daikin

    Reliable in every season

    From frosty mornings to heatwaves, we like to keep your indoor climate steady. Our heat pumps perform even at –28°C and fit just as well in new homes as in renovations. All-electric, future-ready and always energy-efficient.

  • Young man at his desk with his dog, enjoying quiet comfort and smart climate control

    Silence and control, your way

    You barely hear it, but always feel it. Use the app, your voice or set your own schedule. Easy, bright, invisible comfort.

Learn more about our heat pumps and make an informed decision

A heat pump is an efficient low-carbon technology and delivers more energy than it consumes. It uses renewable energy sources such as air, water and geothermal energy to provide heating, cooling and hot water for your home. Indoors, this energy is then released through emitters such as radiators, underfloor heating, heat pump convectors and your hot water system.

Woman at desk with her laptop

Heat pumps convert energy from the outside to the preferred temperature for your home. Initially, a refrigerant in the outdoor heat pump unit absorbs heat from the air, earth or water. The refrigerant enters a compressor, where it is pressurised. Because of the high pressure, the refrigerant becomes hot and, in turn, produces hot water. The hot water can be stored in a tank until it is needed or is circulated via emitters in the different rooms through underfloor heating, radiators or heat pump convectors. When combined with heat pump convectors or underfloor heating, heat pumps can act like air conditioners and also be used for cooling. The cycle is simply reversed, with the indoor units absorbing the heat and the outdoor unit releasing it.

Smiling couple enjoying a relaxed moment in a comfortable living room

A heat pump typically lasts between 15 and 20 years, although this is determined by a number of factors, for instance, maintenance. While heat pumps are a low-maintenance solution, their lifespan will be maximised with an annual check-up by your installer or service partner.

Happy family relaxing on the couch in a perfectly climate-controlled home

Yes, they can, but this depends on the type of emitters you have.

The ideal emitter for cooling is a heat pump convector (also known as a fan coil unit), which cleverly combines heating and cooling in one system.

Couple laughing while playing video games in a cosy room with balanced temperature

A heat pump is ideal for homes of all shapes and sizes and installing a heat pump to warm and cool your home is a smart choice whether it's for a newly built home or a property renovation

Father holding his baby in a warm, peaceful home environment

Air-to-water heat pumps: A fit for any situation

  • Girl reading in a cosy room with warm floors and perfect indoor temperature

    Air-to-water low-temperature heat pumps

    Daikin Altherma low-temperature heat pumps can be used to efficiently cool, heat and provide hot water to newly built homes

  • Son embracing his mother in a welcoming hallway, symbolising the comfort, warmth, and invisible impact of clean, perfectly balanced indoor air by Daikin

    Air-to-water high-temperature heat pumps

    Easily replace your old heating and hot water system with our energy-efficient Daikin Altherma high-temperature heat pumps

  • Young man at his desk with his dog, enjoying quiet comfort and smart climate control

    Air-to-water mid-temperature heat pumps

    Mid-temperature air-to-water heat pumps are an ideal replacement for your old gas boilers offering a renewable solution for cooling, heating and domestic hot water

Not sure which system fits your home?

Let us guide you to the solution that suits your comfort, needs and lifestyle

What our customers have to say about us

Onecta app: control your home climate, anytime

Managing your indoor climate has never been easier. With the Daikin Onecta app, you’re always in control. Wherever you are.

We care for air

Air brings comfort, but true comfort goes further. Daikin solutions use energy from the air to heat and cool your home energy-efficiently. Less environmental impact. Lower energy bills. More peace of mind. For you and your loved ones.

 

Experience the Daikin difference

We've selected some informative and inspirational articles for you to learn more about how Daikin can help you

Explore other smart solutions

We've selected some informative and inspirational articles for you to learn more about how Daikin can help you

Find more information

Take a tour in our virtual showroom

Need help?

Find more information

Corporate Information

Need help?

Find more information

Corporate Information

Need help?

Looking for a new challenge?

Need help?