Our high-performance floor-standing solution heats, cools and purifies the air in your home, throughout all seasons
- Up to A++ energy efficiency for heating and A+++ for cooling means low running costs
 - Heat boost quickly warms up your home
 - Warms the floor for better heat distribution
 - Heat Plus simulates radiant heat for 30 minutes of cosy heating
 - Flash Streamer eliminates allergens and odours
 
Are you an expert and have a specific version in mind? Check our product finder.
        
    
    
    
        
    
    
    
Indoor unit
Advanced floor-standing unit for heating, cooling and purifying air
        
    
    
    
Onecta app
Always in control, wherever you are
        
    
    
    
Outdoor unit
Fits on your roof, wall or in your garden for maximum versatility
        
    
    
    
Service
Enjoy peace of mind with our warranty and service package
        
    
    
    
Remote control
Intuitive and easy-to-use remote control provides total control
Product info
Discover our high-performance floor-standing air-to-air heat pump
Create a more comfortable home with our Perfera floor-standing unit. Advanced heating is combined with cooling and air purification for the ideal indoor climate.
        
    
    
    
Enjoy extra warmth and cosiness
To warm your room, Perfera’s Heat Plus function simulates radiant heat for 30 minutes, providing cosiness just when it’s needed
        
    
    
    
Comfortable and consistent heating
Your home feels extra cosy with Perfera's floor warming function, while its dual airflow directs air up and downwards for consistent, comfortable heating
More information about air-to-air heat pumps
The air-to-air heat pump indoor unit is the part of an air-to-air heat pump system that’s located within the home, and provides the conditioned air into the space.
The choice of an air-to-air heat pump indoor unit depends on your specific needs but it's important to understand how the system works as a whole. There are different air-to-air heat pump systems (also known as air conditioners), each with its own unique characteristics. One of the most popular types used in homes is a split system, which is split into two units: one indoors and one outdoors. While heating, the outdoor unit extracts heat from the outside air and transfers it inside via the indoor unit, or reverse when cooling your home.
There are three types of air-to-air heat pump indoor units:
Wall-mounted units
Wall-mounted models (Stylish, Ururu Sarara, Daikin Emura, Perfera,) come in different sizes and colours to match with your interior.
Floor-standing units
Floor-standing models (Perfera Floor) are compact air conditioner that fit perfectly under a window sill or in a room where the height is limited.
Concealed ceiling units
Concealed ceiling units. If you don't want a visible indoor unit, a concealed air-to-air heat pump can be installed in suspended ceilings or false walls.
There are three options for the placement of the indoor unit of an air-to-air heat pump (also known as air conditioner):
A wall-mounted unit
A wall-mounted unit is ideally positioned above a door or centrally placed in a room. To provide the best comfort, it is not recommended to place the unit above a sofa, the head of the bed or a large closet. This will ensure the airflow can be distributed evenly throughout the room.
A floor-standing unit
A floor-standing unit can be installed underneath a window to avoid that the airflow is blocked. The unit should also not be blocked by furniture to ensure air flows evenly around the room.
A concealed ceiling unit
A concealed ceiling unit is installed in a false ceiling and therefore offers more flexibility thanks to its compact design as only the grilles are visible. The area around the vent should not be blocked by furniture and ideally not directly above a sofa or the head of the bed to ensure optimal comfort.
An air-to-air heat pump (also known as an air conditioner) is typically composed of two units: The indoor and outdoor unit. These are usually called ‘split’ systems.
The split outdoor unit, mounted on an exterior wall or positioned in a garden or on a roof, is the part of an air-to-air heat pump that contains the compressor, propeller fan, circuit board and heat exchanger. The outdoor unit compresses the refrigerant that extracts or emits heat or cold in the room to or from its companion indoor unit.
For your heat pump to function as it should, it is essential that the system is installed correctly. Only an authorised technician should carry out the installation and in a suitable location. The surface must be firm enough to withstand the weight and vibrations of the unit and there must also be sufficient space for airflow and for connecting pipes and power cables. Any plants or shrubs that may be located near your heat pump should be at least a metre away and regularly pruned. The pump should also be installed in a place that’s easy to access for services and other general maintenance.
We often get asked why we can’t put the heat pump inside. Could they not be placed in the loft or conservatory? The answer to this is no. This is because, after a few hours, the heat pump will have extracted all of the warmth from the trapped air, effectively turning this space into a freezer. This is why air-to-air heat pumps need access to the free-flowing outside air.
It is important to differentiate between servicing and cleaning. Air-to-air heat pump maintenance and cleaning can be done by the user, while servicing must be carried out by a professional engineer.
Check your air-to-air heat pump manual and follow any instructions it provides on heat pump cleaning.
- Clean the air supply and return grilles/louvres with a damp cloth and make sure they’re not blocked.
 - Filters can usually be removed and cleaned simply by vacuuming or washing with a bit of lukewarm soapy water.
 - Clean the outdoor unit, gently hose it down to remove dirt and brush it to clear cobwebs. Ensure bits of plants and leaves that may have gathered or have been sucked in the back of the coil are removed. Take care to not damage the fins.
 - Beware – the fins on the coils are very sharp. We recommend using the correct personal protective equipment including gloves.
 - Do NOT use gasoline, benzene, thinner polishing powder or liquid insecticide.
 - Do NOT use water or air that is 40°C or higher.
 - Do NOT use polishing compounds.
 - Do NOT use a scrubbing brush.
 
        
    
    
    
Onecta app: Smart controls from anywhere
Add our easy-to-use Onecta app to your phone for complete control, wherever you go. Alexa or Google Home voice controls let you be hands-free
        
    
    
    
Visualise our air-to-air heat pumps in your own home
Curious about seeing how the indoor unit will look in 3D in your own home?
Experience our showroom online or via virtual reality
Visit our online showroom and visualise our air-to-air heat pumps in different rooms, or, if you have a VR headset, experience our showroom in virtual reality