Air is one of the most essential elements we need to live and yet we fail to recognize the importance of clean air in indoor environments.
It has an impact on people’s health and performance at work, or on their everyday life activities. The more contaminated the air indoors is, the quicker people succumb to illnesses, allergies and rising stress levels. Even when the concentration of pollutants in a room is very subtle.
Enclosed environments significantly contribute to air pollution exposure, as people spend almost 90% of their time indoors. In addition, indoor air is usually 2 to 5 times more polluted than outdoor air, mainly due to the lack of proper air exchange.
Especially since the pandemic, it has become clear how important air exchange is as it helps dilute or even bring contaminant concentrations down to zero in enclosed spaces.
Natural ventilation vs. Mechanical ventilation
Ventilation should always be guaranteed in indoor environments as it helps to address all the above-mentioned issues related to poor indoor air quality.
What are the available options to ensure proper ventilation in a building, though?
One is usually natural ventilation: introducing outdoor air in enclosed spaces by removing barriers such as opening windows or doors. It allows fresh indoor air to replace exhaust air naturally. While it might seem an easy and simple way to make air exchange in enclosed environments happen, it also has its downsides.
Among them there are:
- thermal dissipation;
- no filtration of the newly introduced air indoors;
- higher energy consumption;
- no active or direct control over air exchange.
In fact, while air exchange might be easily guaranteed to some extent with natural ventilation, the thermal conditions of the environment being ventilated are inevitably going to change. When air is introduced at a different temperature than the indoor environment, the space will not be able to retain warmth during fall and winter and coolness in spring and summer. This forces climate control systems to work harder to achieve the target indoor temperature which in turn consumes more energy.
Secondly, there is the aspect related to the lack of filtration. With natural ventilation, the newly introduced air that replaces the exhaust air might not be clean enough and contain pollutants such as pollen and other contaminants.
On the contrary, mechanical ventilation ensures perfect thermal control and no thermal dissipation thanks to energy recovery technology. It can transfer heat and moisture from the airflow being extracted to the airflow being introduced in the premises.
And finally, mechanical ventilation systems can ensure high levels of air filtration, making sure that only clean air is introduced in buildings.
Mechanical ventilation in existing buildings
It is a fact that mechanical ventilation contributes greatly to high indoor quality levels in indoor environments.
While it’s mostly a standard in Northern European countries, where buildings are usually designed to be thermally insulated with minimal energy consumption, mechanical ventilation is not overly present in the rest of the European building stock.
Most of the existing buildings (schools, public offices, light-commercial buildings or even residential buildings) were built decades ago without proper ventilation systems and can nowadays not even accommodate a new installation due to structural restrictions.
Luckily, technology is constantly evolving and the air conditioning sector is now able to offer compact solutions to make installation in existing buildings possible and easy. With this vision in mind, Daikin is about to launch a design that gives customers the possibility to upgrade their building with a modern system, an all-in-one solution able to provide ventilation, cooling, heating and dehumidification. This will help raise indoor air quality levels in existing buildings and make them a healthy environment for occupant.
Every year in May we will provide an update of this text.
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com