Daikin has announced the launch of the Perfera FTXM-R series of wall-mounted air conditioners. Combining proven technology with brand new design features, Europe’s best-selling home air conditioning solution is set to break new records over the coming months.
The new Perfera FTXM-R series offers an all-in-one heating, cooling and clean air solution housed in an elegant indoor unit whose contemporary form and flowing lines will grace any interior. Now housed in an even smaller unit measuring 30 mm less than previous versions, the Perfera FTXM-R/RXM-R blends in effortlessly.
The new unit is easy to install, with near-silent operation offering an unobtrusive solution and comes in a wide range of sizes. Incorporating the latest air purifying and heating technology, together with new voice control abilities, the new FTXM-R series offers maximum comfort, performance and connectivity with best-in-class seasonal energy efficiencies of up to A+++ in cooling and heating.
Technology-driven comfort
Building on the advanced technology of previous models, the latest Perfera wall-mounted unit introduces several important new features.
A new ‘heat boost’ function in the outdoor unit quickly heats homes when starting up, reaching the set temperature 14% faster than a regular conditioner.
The next generation Perfera unit has been designed with a wider flap to give a stronger airflow, while the 3D air direction feature distributes hot or cold air more evenly for all-round room comfort.
Additionally, the two area motion detection sensor deflects air away from people and auto-switches to a more energy efficient setting when no movement is detected in the room.
A new design heat exchanger and fan ensures reliable performance, improved heat transfer and superior energy efficiency.
Breathe easy with Daikin’s unique flash streamer
Daikin’s advanced flash streamer technology protects homes by filtering the indoor atmosphere to deliver pure, clean air. The integral titanium apatite deodorising filter captures and neutralizes unpleasant odours such as tobacco and pet smells.
The silver allergen removal and air purifying filter captures allergens such as pollen to ensure a steady supply of clean air.
Connectivity and control
The new Perfera offers outstanding connectivity. The Daikin residential controller, accessible through Daikin’s downloadable app via a local network or internet connection, has been supplemented by a new voice-activation facility. Key functions including temperature set points, operation modes, fan speed and more, can be controlled from anywhere using Amazon Alexa or Google Assistant.
Easy installation and commissioning
The wide range of sizing options, from the 15-class up to 71-class models, provides maximum flexibility in system specification. The piping diameter of the 42-class type has been unified with the
35-class units for increased system compatibility. With the new integral Perfera PCB and WLAN connection, commissioning is both simple and fast.
In good company
The Perfera series is a part of the Bluevolution family of products. Operating on R-32 with low environmental impact, this latest addition to the Daikin portfolio complies with both existing and planned F-Gas regulations to provide a future-proof sustainable climate solution for heating, cooling, and air purification in the home.
Every year in May we will provide an update of this text.
Press release
-
Perfera wall mounted FTXM-R_Press Release_DEUEN20-010_EnglishZIP | 237.17MB
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com