Technology meets design in Daikin’s new Perfera FVXM-A floor-standing air conditioner to create the ideal climate solution for the home all year round. Combining heating and cooling into one, the new Perfera incorporates unique new features to deliver the ultimate in comfort and performance.
Easy to use and install, the compact Perfera FVXM-A floor standing unit conceals a technology powerhouse designed to deliver a powerful performance with top energy efficiencies up to A++ in heating and A+++ in cooling, while introducing a new sense of wellbeing and personal comfort to any living space. Its sleek appearance and flowing lines blend well with any interior to give a contemporary look and feel.
Virtually inaudible in use, incorporating clean air technology and intelligent controls now also incorporating new voice commands, the new Perfera FVXM-A works around the homeowner’s daily needs without disrupting their peace and quiet. New heat boost and airflow features create a feeling of cosiness whatever the weather outside.
Quietly efficient
The new Perfera FVXM-A blends into the background while efficiently getting on with its job. Practical yet understated, the new indoor unit incorporates a stylish designed front panel that lets users know what is going on. The unit’s light (Daikin eye) changes colour to reflect the operating status and can be dimmed or turned off if preferred. The turbo fan keeps the indoor ambient temperature constant at a sound level that is practically inaudible. The Perfera FVXM-A also provides a night mode setting which automatically sets the temperature 2˚C cooler when heating and 0.5˚C warmer when cooling ensuring a restful night’s sleep.
Winter comfort
Everyone likes to feel cosy when it is cold outside. The new Perfera FVXM-A has been designed with an emphasis on heating. Three new advanced features have been incorporated to create an extra sense of wellbeing and comfort.
A new automatic heat boost function introduced for the outdoor units quickly heats homes from system startup, allowing set temperature to be reached 14% faster than a regular air conditioner.
At the touch of a button, the heat plus setting creates the feeling of comfort by simulating radiant heating, switching off again after 30 minutes.
Also new to the latest generation Perfera is a floor warming function which optimises convection by distributing hot air from the bottom of the unit and ensures feet stay toasty warm.
Like its predecessors, the new Perfera FVXM-A incorporates Daikin’s unique dual airflow, which is easily set via remote controller, ensuring even air distribution around the room. The Perfera’s wide upper flap allows direction of hot or cool air as required.
Together, these features allow the Perfera FVXM-A to achieve high energy efficiencies while creating an inviting ambience.
A breath of fresh air
Daikin’s Flash Streamer technology, combined with a titanium apatite deodorising filter delivers cleaner air, protecting against airborne particles and allergens for a healthier indoor environment.
Putting the user in control
The Perfera FVXM-A is easy to adjust with the infrared remote control supplied as standard and can also be managed using a smartphone with Daikin’s downloadable app. Using the new voice control feature, the system settings can also be activated via Amazon Alexa or Google Assistant from any room, making it easy to regulate the internal climate wherever you are.
Freedom for installers
The system’s compact size means the outdoor unit can be installed easily on the roof, terrace or against an outside wall, while connectivity to the indoor units is provided as standard with the new PCB featured in the latest model. The Perfera FVXM-A can be used in a single room set-up, with one indoor unit connected to one outdoor unit or in a multiple room configuration with up to 3 indoor units linked to a single outdoor unit.
The range has been extended to provide 4 capacities, with 20, 25, 35 and 50 class versions available. The Perfera FVXM-A is also the best choice for cold climates down to -25C with 25-35 class available
Thinking for the future
The Perfera FVXM-A is the latest in Daikin’s Bluevolution range of home heating solutions. Operating on R-32, the new system complies both with existing and future F-Gas regulations as a low GWP solution.
Every year in May we will provide an update of this text.
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 58 04 82 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 46 23 21 Mail: kakinaga.d@bxl.daikineurope.com
Press release
-
DEUEN20-009ZIP | 382.68MB