Skip to main content

Improve your Indoor Air Quality

The air purifying technology of Daikin airconditioners delivers clean air which provides the perfect foundation for optimal comfort.

Couple laughing while sitting on a couch with popcorn.

Flash Streamer

The massive streamer discharge hits the allergens and hazardous chemical substances, decomposing and fragmenting their surface proteins, which are then destroyed through oxidation.

During the test allergens were placed on the electrode of the streamer discharge unit and then photographed through an electron microscope after being irradiated.

(Testing organization: Yamagata University and Wakayama Medical University)

allergens photographed through an electron microscope after being irradiated.
Boy playing with a toy car on the floor.
Boy playing with a toy car on the floor.

Titanium apatite deodorising filter

Daikin’s titanium apatite deodorising filter removes airborne dust particles and captures the odours of tobacco and pets, for example. It also traps and even deactivates harmful organic chemical substances to ensure you enjoy a steady supply of clean air.

Schema titanium apatite filter

How does it work?

1. When UV light shines on the titanium dioxide, electrons are released at its surface.

2. The electrons interact with water molecules in the air, breaking them up into hydroxyl radicals, which are highly reactive, short-lived, uncharged hydroxide ions

3. These radicals attack bigger pollutant molecules, breaking apart their chemical bonds and turning them into harmless substances such as carbon dioxide and water.

Woman looking outside while holding the curtains.
Woman looking outside while holding the curtains.

Silver allergen removal and air purifying filter

Do you suffer by seasonal allergies or allergies of pets and dust mites? 

Then Silver allergen removal and air purifying filter is your solution, because it captures allergens such as pollen and dust mites. The filter suppresses pollen and mites for 99% or more.

Thanks to its high quality and remarkable efficiency, replacement of the filter is needed just once every 6,5 years. 

Workings of the automatic filter cleaning technology. Illustration.

Automatic filter cleaning 

Just like vacuum cleaners, air conditioners use filters to clean the air as it passes through the unit. 

And the more particles collect in the filter, the less efficiently it works. But with the Ururu Sarara’s state of the art self-cleaning technology, that is a thing of the past. Not only is that less work for you, it is less work for the Ururu Sarara - it keeps a constantly stable air flow rate while using 25% less power.

Close up on Daikin Ururu Sarara unit.
Close up on Daikin Ururu Sarara unit.

Ventilation for fresh air 

Unlike a conventional air conditioner, the Ururu Sarara brings fresh, conditioned air into the room. 

The Ururu Sarara is the very first residential heat pump system that - because of its powerful ventilation capacity of 30 m3/h - can fill a room of more than 26 m2 with fresh air in less than two hours.

And the incoming air is brought in at the desired temperature without thermal loss.

Flash streamer

Using electrons to trigger chemical reactions with air molecules, the flash streamer captures mold and allergens.

About Flash Streamer

Titanium apatite filter

Daikin’s titanium apatite deodorising filter removes airborne dust particles and captures the odours of tobacco and pets.

About Titanium apatite filter

Silver filter

Silver allergen removal and air purifying filter captures allergens such as pollen and dust mites.

About Silver filter

Ventilation

Fresh air and conditioned air with the windows closed thanks to the unique technology of Ururu Sarara.

About fresh air input
bg-image

Top air treatment through unique filtration and fresh air input

We live in times when we are getting more concerned about the environment we live in and the air we breathe, especially at home. 

How can we take care of the indoor air quality, among all other things? 

It is actually more than easy by investing into the state-of-the-art air-conditioning solutions by Daikin.

Daikin Stylish filters: Air Filter, Titanium Apatite, Silver allergen removal filter and Flash Stramer. Illustration.

Daikin Solutions

Click on one of the features below to find the unit you need

Humidification and fresh air in your home: Ururu Sarara

Cooling energy efficiency up to A___.jpg Heating energy efficiency up to A___.jpg
Fresh air ventilation
Automatic filter cleaning​
Flash streamer
Titanium apatite deodorising filter
Air filter

Minimalism and technology united: Stylish

Cooling energy efficiency up to A___.jpg Heating energy efficiency up to A___.jpg
Flash streamer
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

Stylish: Elegant on the outside, smart in the inside - even at -25°C!

Cooling energy efficiency up to A__.jpg Heating energy efficiency up to A___.jpg
Flash streamer
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

If you value top design: Daikin Emura

Cooling energy efficiency up to A___.jpg Heating energy efficiency up to A__.jpg
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

If you value a high performance solution: Perfera

Cooling energy efficiency up to A___.jpg Heating energy efficiency up to A___.jpg
Flash streamer
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

Perfera: high performance even at -25°C

Cooling energy efficiency up to A__.jpg Heating energy efficiency up to A___.jpg
Flash streamer
Titanium apatite deodorising filter
Air filter

Comfort and efficiency for everyone: Comfora

Cooling energy efficiency A__.jpg Heating energy efficiency up to A__.jpg
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

Comfora, discreet wall mounted unit even at -25°C​

Cooling energy efficiency A__.jpg Heating energy efficiency up to A__.jpg
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

Offering good value for money: Sensira

Cooling energy efficiency up to A__.jpg Heating energy efficiency up to A_.jpg
Titanium apatite deodorising filter
Air filter

Ideal for attics: Perfera

Cooling energy efficiency up to A___.jpg Heating energy efficiency up to A__.jpg
Flash streamer
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter

Perfera: for optimal heating comfort even at -25°C​

Cooling energy efficiency up to A__.jpg Heating energy efficiency up to A__.jpg
Flash streamer
Silver alergen removal filter
Titanium apatite deodorising filter
Air filter