With the new Daikin Emura, Daikin brings together the best of design and technology to help you achieve your perfect indoor climate: Daikin Emura keeps you cool in summer, and warm in winter. The new air conditioning unit also surprises with its curved design – pure elegance!
“Daikin Emura blends harmoniously into your interior”
Daikin Emura includes a wall mounted indoor unit, remote control and outdoor unit. Beautiful and intelligent design that blends harmoniously into your interior: high-end yet affordable. Daikin Emura will even make your walls proud.
Remarkable design
With a width of only 90 cm, Daikin Emura is proud to be different. Thanks to its curved panels, the indoor unit has a unique 3D shape. The curved lines refer to the harmonised airflow, but also create a visual effect in your interior: they create shadows and make Daikin Emura really come to life.
“A wall mounted air conditioning unit always has a visual impact. I believe it can also be a design statement. Using shadows is the most natural way to make product and interior design much more interesting”, reveals Hiroyasu Kosuge, Daikin Emura brand designer.
The remote control has the same sleek design and fits your hand perfectly. Both the indoor unit and the remote control are available in silver, matt white and matt black. The redesigned outdoor unit comes in ivory white.
Optimised air distribution
It goes without saying that a room only needs to be cooled or heated when you’re actually in it. Daikin Emura uses an intelligent thermal sensor and specially designed flaps to (re)direct the airflow and ensure a constant and harmonised temperature throughout the room. Thanks to the new heat boost function, Daikin Emura quickly heats a room when starting up, ensuring the set temperature is reached faster
Whisper quiet operation
A Daikin Emura air conditioner runs so quietly you’ll almost forget it’s there. A specially designed fan optimises the airflow for high performance levels at low sound levels, making Daikin Emura practically inaudible in operating mode.
Better indoor air quality
With built-in air purifying filters and Flash Streamer technology, Daikin Emura captures dust particles, breaks down allergens and removes bothersome odours, providing you with better, cleaner air. That’s how the Daikin Emura air conditioning unit keeps your home healthy.
User-friendly control
Control the indoor climate with ease. The new remote control introduces a simplified design with strong focus on the most important functionalities. You can easily access all other features via the self-explanatory menu or from anywhere at any time with the intuitive Onecta app on your smart devices.
Maximum efficiency
Whether it’s extremely hot or cold outside, you expect your air conditioner to perform all year long in the same stable way. Daikin Emura is engineered to perform every season and provide year-round comfort in the most energy-efficient way. Your guarantee for best-in-class performance with seasonal efficiency values up to A+++ in cooling and heating, resulting in a low environmental impact and low energy bill.
Two prestigious awards
The new Daikin Emura blends elegant design with state-of-the-art technology and outstanding efficiency. No wonder it was honoured with this year’s Red Dot Product Design Award and iF Design Award – two of the most prestigious design awards in the world that reward remarkable product innovation.
DAIKIN EMURA FTXJ-AW MATT WHITE
DAIKIN EMURA FTXJ-AS SILVER
DAIKIN EMURA FTXJ-AB MATT BLACK
-
Daikin Emura 3_B2C_Press release_DEUEN22-004_EnglishZIP | 711.44MB -
Daikin Emura 3_B2B_Press release_DEUEN22-004_EnglishZIP | 718.41MB
Every year in May we will provide an update of this text.
About Daikin
Daikin Europe N.V.
Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580 482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com