Skip to main content

Daikin launches sound enclosure for VRV and Sky Air to offer customers one-stop shopping

05/05/2021

The intelligent approach to sound reduction

Strict sound regulations typically apply in inner-city or residential areas where buildings are built closer together. This means that choosing highly-efficient HVAC equipment to decarbonise the premises might pose challenges to sound regulations. The latest-generation commercial heat pumps are already designed for quiet operation, however for sound-sensitive projects, this new low-sound enclosure further reduces sound power levels by up to 10 dB(A). Additional calculations of sound, capacity or efficiency are not needed since all essential values are factory measured.

Available from May onwards, the new Daikin sound enclosure specifically designed and tested for Sky Air Alpha-series, Sky Air Advance-series and VRV 5 S-series outdoor units reduces the sound power level by up to 10 dB(A).

 

Designed to be discreet

The Daikin sound enclosure has a highly aesthetic finishing and a smooth surface. An anthracite colour (RAL 7016) underlines its unobtrusive looks. Its tailor-made design fits our outdoor units perfectly and keeps dimensions to a minimum.

Tested and approved: values that you can rely on

Daikin sound enclosures offer a solution specifically designed for the low height Daikin Sky Air and VRV heat pumps. Thoroughly factory-tested sound power (ISO 3744), efficiency and capacity guarantee flawless system performance. This makes it possible to determine in advance how the installed system will operate. It also simplifies the layout and planning because separate calculations are not required.

Sound power values in both cooling and heating according to ISO 3744 are available, as well as sound pressure and low noise operation mode values.

The solution that meets the need

The sound enclosure is optimised so that airflow and capacity are as close as possible to the standard conditions. Separate air inlets and outlets combined with the perfect fit of the enclosure prevent air short-circuiting for efficient sound reduction and minimised pressure drop.

The new sound enclosure is also easy to install: as a self-supporting unit, it can be placed on any flat surface. The side panels of the sound enclosure can be conveniently unlocked with quick-release buckles for easy access to key components when maintenance work is required.

If needed, an optional drain pan and heater are available. Existing outdoor units can also be upgraded with the sound enclosure.

For more information visit: https://www.daikin.eu/en_us/products/ekln-a.html

 

 

Every year in May we will provide an update of this text.

About Daikin

Daikin Europe N.V.

Daikin Europe is a subsidiary of Daikin Industries Ltd. and the leading provider of heating, cooling, ventilation, air purification and refrigeration solutions in Europe, the Middle East and Africa. The company designs, manufactures and brings to market a broad portfolio of equipment, as well as tailor-made solutions for residential, commercial and industrial purposes. To date Daikin Europe has over 12,000 employees working at more than 59 consolidated subsidiaries. It has 12 major manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Turkey, Austria and the UK. The headquarters of the Daikin Europe group are in Belgium, Ostend. The company was established in 1972, production in Europe started in 1973.

About Daikin Industries Ltd.

Based in Osaka, Japan, Daikin Industries employs over 89,000 people worldwide. The global company is market leader for heat pump and air conditioning systems, as well as air filtration. It is the only air conditioning manufacturer in the world that researches, develops and produces all important system components, such as refrigerants, compressors and electronics, in-house. The company achieved € 23.7 billion sales turnover in financial year 2021 (1 April 21 – 31 March 22).
 

Media Contacts Daikin Europe N.V.

Sofie Sap – T.:  +32 472 580 482 Mail: sap.s@daikineurope.com

Daisuke Kakinaga – T.: +32 465 462 321 Mail: kakinaga.d@bxl.daikineurope.com

Related articles