Brussels, July 2024 – Daikin launches two new plug-and-play air purifier models to effectively improve indoor air quality and give access to real-time insights on air quality. The models MCK70Z and MC80Z connect to Daikin’s Onecta app, which allows users to control, monitor and schedule air purification through a smartphone or tablet. The app gives insights into both indoor and outdoor air quality data. Indoor air quality is measured through the sensors integrated in the air purifiers, while outdoor air quality data is made available via Google Maps Platform.
Improving indoor air quality of homes and offices
With growing awareness of pollution and allergens, indoor air quality has never been more important. Daikin’s air purifiers effectively capture and clean indoor air from airborne particles, including fine particulate matter such as PM2.5, pollen, pet hair and other harmful substances. Both units are equipped with patented ‘streamer’ technology that capture and decompose fine harmful particles, ensuring that the air is cleaner and healthier. With a sleek and stylish design, the MCK70Z and MC80Z units easily fit into any space and interior. They are particularly suited for homes and light commercial spaces such as schools, offices, shops and hotels. Like the previous air purifier models, they have long filter lifetimes of 10 years, which saves users the trouble and expense of replacing filters frequently. Their whisper-quiet operation makes them well-suited for use in bedrooms and any space that requires concentrated work.
Full control over indoor air quality
Both units come with a WLAN integration and can be controlled, via smartphone or tablet, on the Daikin Onecta app, which is the same app used for managing Daikin’s air-to-air & air-to-water heat pumps. Controls include real-time monitoring of the indoor and outdoor air quality, visualisation of PM2.5 presence, management of the units and scheduling the air purification.
Daikin’s work with Google Maps Platform
While the PM2.5 sensors in our Daikin air purifiers show the indoor air quality, the outdoor air quality information is brought to our users thanks to our collaboration with Google Maps Platform.
By integrating outdoor air quality & pollen data from Google Maps Platform together with Daikin’s indoor air quality data, the quality of both indoor and outdoor air is simply available through the Daikin Onecta App. This ensures our customers have high awareness about the air quality they breathe. As indoor air quality (IAQ) experts ourselves, with over decades of experience in perfecting the air, our mission is to provide both indoor & outdoor air quality data so that customers can be better informed.
The info on outdoor air quality and pollen levels is available via the Daikin Onecta app.
MCK70Z – the ultimate air purifier with humidification
The MCK70Z additionally comes with a humidification function, making it an ideal solution for homes and light commercial spaces with low humidity levels.
It is designed to cover a surface of up to 96m² (calculated in accordance with JEM1467) with CADR of 375 m³/h, making it ideal for use in medium-sized rooms, including living rooms and offices.
Daikin Air Purifier MCK70ZW & MCK70ZH
MC80Z – a powerful air purifier covering large surface area
The MC80Z is the other new top-of-the-line air purifier that offers exceptional performance and is designed to cover an applicable surface of up to 124m² (calculated in accordance with JEM1467) with CADR of 480 m³/h, making it ideal for use in medium-sized rooms as well as larger spaces such as conference rooms, classrooms or libraries.
Daikin Air Purifier MC80Z
Watch this video to learn more about Daikin air purifier technology
References and abbreviations:
1) CADR= Clean Air Delivery Rate
2) dB(A) = A-weighted decibels consider the frequencies the human ear doesn't perceive
3) WLAN= Wireless Local Area Network
Copyrights pictures: Daikin Europe
About Daikin
About Daikin Europe N.V.
Daikin Europe N.V. is a subsidiary of the global group Daikin Industries, and the leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC&R) technology in Europe, Middle East and Africa. Daikin designs, manufactures, and brings to market a broad portfolio of products, maintenance services as well as turnkey solutions for residential, commercial, and industrial purposes. To date Daikin Europe has over 13,700 employees across more than 57 consolidated subsidiaries. It has 14 manufacturing facilities based in Belgium, the Czech Republic, Germany, Italy, Spain, Austria, the United Kingdom, Turkey, the United Arab Emirates, and the Kingdom of Saudi Arabia. The headquarters of the Daikin Europe group are in Ostend, Belgium. The company was established in 1972, production in Europe started in 1973.
About Daikin Industries Ltd.
Daikin Industries was founded in 1924, in Osaka, Japan and is celebrating its 100th anniversary this year. The global group employs over
96,000 people worldwide and is the market leader for heat pump and air conditioning systems, as well as air filtration. It is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning and refrigeration equipment, as well as refrigerants in-house. The company achieved € 28.2 billion sales turnover in fiscal year 2022 (1 April 2022 – 31 March 2023).
Read more on www.daikin.eu and www.daikin.com.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580482
Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462321
Mail: kakinaga.d@bxl.daikineurope.com
Media Contact for product inquiries Daikin Europe N.V.
Jonas Bosman – T.: +32 496 95 53 65
Mail: bosman.j@daikineurope.com
Ayushi Saxena – T.: +32 477 55 01 67
Mail: saxena.a@bxl.daikineurope.com