Brussels, 16 October 2025 – Daikin’s new factory in Poland designed by Takenaka has been recognized by the PLGBC Green Building Awards for its building design and various ecological technologies such as a building management system, rainwater retention and heat pumps. The award ceremony took place on October 9 in Warsaw (Poland) at the 15th edition of the Green Building Summit, Poland’s premier event dedicated to sustainable construction and architecture run by the Polish Green Building Council.
Sustainable Industrial Building category
The Polish Green Building Council (PLGBC) is a non-governmental organisation part of World Green Building Council. Takenaka Europe and Daikin Europe are the joint winners of a PLGBC Green Building Award 2025 in the Sustainable Industrial Building category for Daikin’s new residential heat pump factory in Ksawerów near the city of Łódź (central Poland).
“We are proud that Takenaka and Daikin are the joint winners of a PLGBC Green Building Award 2025. Our new residential heat pump production site has been beautifully designed by Takenaka and has various state-of-the-art ecological building features,” says Yasuto Hiraoka, President of Daikin Manufacturing Poland.
Innovative building features
“The primary design challenge was to provide sunlight to the east-facing glazed façade. The glazing angle eliminates the need for blinds or shutters. Passive solar control allows for daylight while preventing overheating and glare. The innovative climate-responsive façade solution exemplifies sustainable design and showcases Daikin’s energy-efficient products,” says Kentaro Fujimoto, Design manager of Takenaka Europe.
Another innovation highlight is the integrated stormwater retention system for the 320,000 m2 manufacturing site. After initial treatment, stormwater is directed to two large, underground retention tanks. This allows for controlled drainage of water into a drainage ditch, reducing the risk of flooding or overloading the stormwater infrastructure.
Social value and accessibility
The zigzag facade of the office reduces solar heat gain, achieving large glazed areas with low environmental impact. The design expresses environmental considerations and social responsibility through diverse visual expressions when viewed from different angles.
“It combines efficiency and architectural expression, embodying the building's core environmental principles, serving as a functional, architectural element that manifests the building's values,” adds Kentaro Fujimoto, Design manager of Takenaka Europe.
Reducing energy consumption
“To achieve carbon neutrality in the future, our factory is implementing electric heat pumps and optimized ventilation, using a hybrid air/water cooling system designed for low temperatures in Poland, with waste heat recovery and innovative engineering for sustainable development,” says Yasuto Hiraoka, President of Daikin Manufacturing Poland.
Heat pumps obtain energy from outside air, which allows for significant reduction of heating costs and CO₂ emissions. It provides stable heating of halls and offices and the possibility of cooling in the summer, which increases work comfort and supports the sustainable development of the plant.
The building management system (BMS) is an advanced tool supporting energy-efficient and ecological building management. It allows for precise control of energy consumption, optimizing the operation of heating, ventilation and lighting systems, which translates into a significant reduction of operating costs. BMS integrates monitoring of technological gases with detectors and shut-off valves, ensuring safety and minimizing the risk of failure. The system supports sustainable development, allowing for effective utilities management and emission reduction.
Occupant health and well-being
Sufficient natural light and ventilation have been incorporated into the workspace with temperature and humidity control. “Natural light has been shown to improve mood, productivity and overall well-being. While optimal ventilation helps maintain indoor air quality, reducing the risk of respiratory illnesses and increasing comfort,” adds Yasuto Hiraoka, President of Daikin Manufacturing Poland.
Elements of nature are also integrated into the workspace through the use of plants, natural materials and views of greenery. This ‘biophilic’ design has been linked to reduced stress, increased creativity and improved cognitive function among employees.
The facility uses energy-efficient LED lighting with a lighting control system that allows lighting scenes that improve visual comfort, reduce eye fatigue and have a positive effect on the circadian rhythm of users. High-quality sound-absorbing materials were used in the buildings in walls, ceilings and office partitions.
The building was designed with full accessibility for people with limited mobility in mind. It is equipped with ramps, elevators, suitably wide passages and toilets adapted to the needs of people using wheelchairs. This approach supports inclusiveness, equal treatment and comfort of all users.
Reduced water consumption
Water consumption is reduced by using a landscape plan that does not require a permanent irrigation system for outdoor plantings.
There’s a system that circulates and reuses the heating and cooling water for the heat source. The system measures and aggregates water consumption in buildings and outdoor areas, tracking monthly and annual consumption. It enables collaboration on water management with facility operators and allows aggregation by consumption and area. The system also educates employees and visitors by visually displaying water data on monitors.
About Takenaka Europe
Takenaka Europe GmbH delivers integrated architecture, engineering, and construction services, operating across 13 branches in Europe. Founded in 1973, the company is a subsidiary of Takenaka Corporation, which has over 400 years of building heritage rooted in Japanese master builder tradition.
Takenaka Europe applies a design-build approach that combines planning, design, and execution within one organization. This method supports coordinated project delivery and consistent quality across a wide range of building types and sectors. The company employs more than 640 employees and operates under certified systems, including ISO 9001 for quality management, along with established procedures for health, safety and environmental protection. Headquartered in Düsseldorf, Germany, Takenaka Europe contributes to the group’s global mission: “Contribute to society by passing on the best works to future generations.”
About Daikin Europe N.V.
The Daikin Europe Group is a leading provider of heating, cooling, ventilation, air purification and refrigeration (HVAC-R) technology in Europe, Middle East, and Africa. Daikin Europe caters to a diverse customer base within this region by designing, manufacturing, and marketing an extensive range of products, maintenance services, and turnkey solutions tailored for residential, commercial, and industrial applications. The company employs over 13,800 employees through 58 subsidiaries and operates 15 manufacturing sites in Europe (12), Turkey (1) and the Middle East (2). Daikin’s refrigeration products are available under the Daikin, Tewis, Zanotti, Hubbard, and AHT brands. Headquartered in Ostend, Belgium, for over 50 years, the Daikin Europe group is a subsidiary of the global group Daikin Industries.
About Daikin Industries Ltd.
Daikin Industries (DIL) is a global leader in heat pump, air conditioning and air filtration technology. The company employes over 100,000 employees worldwide. Founded in Osaka in 1924, it is the only manufacturer in the world that develops and manufactures heating, ventilation, air conditioning, and refrigeration equipment, as well as compressors and refrigerants in-house. Daikin was named one of the world’s top 100 most innovative companies by Clarivate (UK) and LexisNexis (USA), recognized for its leadership in technology research and intellectual property patents. For its fiscal year 2024 Daikin reported a record sales result of € 28,98 billion sales (1 April 2024 – 31 March 2025).
Read more on www.daikin.eu and www.daikin.com.
Media Contacts Daikin Europe N.V.
Sofie Sap – T.: +32 472 580482 Mail: sap.s@daikineurope.com
Daisuke Kakinaga – T.: +32 465 462321 Mail: kakinaga.d@bxl.daikineurope.com