Skip to main content

When trying to make a direct connection to the adapter ([AP] mode), the adapter is not visible in the available Wi-Fi networks list of the phone/tablet.

Try the following:

  • Follow the setup guide in the application1.
  • Please check that you are close enough to your WLAN adapter (< 2m line of sight). The range of the WLAN adapter can be reduced significantly by interference on the Wi-Fi channel.
  • Switch to [RUN] mode and return to [AP] mode by pressing the [MODE] button. That way, the adapter will switch to another Wi-Fi channel (1-11). Repeat if necessary.

1 The setup guide (“Add adapter”) can be accessed through the main menu.

FAQ onlinecontroller direct-connection to the adapter ap mode the adapter is not visible