Skip to main content

The programmed timer action is not executed at the programmed time.

The timer actions are executed according to the WLAN adapter clock. You can check the current WLAN adapter date and time in the application in the adapter settings1.

Make sure that the time zone has been set correctly for every WLAN adapter.

1 To access the “Time” information:

  1. Select the unit on the smartphone application.
  2. Go to the adapter settings (“Gear” icon in top right corner).
  3. Select “Time”.
FAQ onlinecontroller programmed timer action is not executed at the programmed time