Skip to main content

On the FTX20/25/35J2V1B and FTXL, I cannot set temperatures below 14°C when in heating mode

On this model, the lowest temperature that can be set (with Infrared Remote controller, wired remote controller and smartphone application) is 14°C.