A. To setup the adapter to connect to your home network, please follow the setup guide1.
B. To access the wireless connection settings, make sure that the smartphone is connected directly to the WLAN adapter (AP mode)2. Otherwise, the wireless connection settings are not available 3.
1 The setup guide (“Add adapter”) can be accessed through the main menu
 
        
    
    
    
2 To connect to the adapter directly, please follow the setup guide1.
3 To access the “Wireless connection” settings:
- Connect to the adapter in AP mode and select “Configure the wireless connection” on the Home screen.
- Select the network you want to connect to.
- Here you can change the “Advanced network settings” or change the password.