Could the system shut down the air conditioning or the domestic hot water tank?
- Yes, the air conditioning can be shut down by the system. The domestic hot water tank can’t be completely shut down as it always warms up. However, it can heat purely using the electric heater.
| Priority | Air conditioning mode | Can the outdoor unit provide both functions? | Description |
Domestic hot water | Cooling | No | Domestic hot water only, the air conditioning is on standby. |
| Heating | Yes | Domestic hot water and air conditioning work at the same time. | |
| No | Domestic hot water only, the air conditioning is on standby. | ||
Air conditioning | Cooling | No | Air conditioning only, domestic hot water is heated by the electrical heater. |
| Heating | Yes | Domestic hot water and air conditioning work at the same time. | |
| no | Air conditioning only, domestic hot water is heated by the electrical heater. |