To suppress the laundry's damp odor, it is ideal to dry it within 5 hours!
The most important thing to prevent the generation of the damp odor is the "time from the end of washing to the drying". Moraxella bacteria explosively grows after about 5 hours, so if you can dry it within 5 hours, you can suppress the damp odor to some extent. What we would like to keep in mind here is the trick of drying clothes in the room. First, it is important to hang it in a well-ventilated place. It is assumed that many people hang it on the curtain rail, but it is the worst place because it is easy for moisture to accumulate at the window and there are many germs.
And, we also devised how to dry. You can quickly dry the clothes by hanging the long one on the outermost side of the clothes hanger, the "arch drying" that hangs the short one in the middle, or the "ghost drying" that puts only the sleeve part of the long-sleeved shirt on another hanger... Considering the growth of bacteria, it is recommended to use a dehumidifier or air conditioner equipped with an air cleaning function. If you're worried about odor, please give it a try, as the laundry odor can be suppressed with a little effort like this.