I have multiple adapters in the same wireless network. I do not know anymore which WLAN adapter is matching with which unit on my Daikin Online Controller smartphone application.

To be able to trace back the WLAN adapter that is connected to a certain unit on the smartphone application, you can use the connection test function1.

When this function is enabled, the LEDs on the matching WLAN adapter will start blinking for about 3 minutes.

 To access the “Connection test”:

  1. Select a unit on the smartphone application.
  2. Go to the adapter settings (“Gear” icon in top right corner).
  3. Select “Connection test”.
FAQ onlinecontroller programmed timer action is not executed at the programmed time