Skip to main content

Pure air, because we care

With Daikin air purifiers, we promise you air that is cleaner, healthier and fresher.

Effective for cleaning the air and removing:

Viruses

Allergens

Dust particles

Odours

Tested by

IPL

99.98% of coronavirus removed in 2.5 minutes*
As tested by Institut Pasteur de Lille

According to tests performed in the laboratories of the Institut Pasteur de Lille, Daikin’s air purifiers remove more than 99.98% the human coronavirus HCoV-229E in 2.5 minutes*. This virus is of the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic.

The units have also been evaluated as 99.93% effective against the H1N1 virus in 2.5 minutes*.
H1N1 is the virus causing common flu.
This means Daikin’s air purifiers are an additional measure in the fight against respiratory diseases. Our compact plug-and-play purifiers, whose effectiveness is achieved through a combination of the high performance electrostatic HEPA filter, which traps the virus, followed by an intense exposure to Daikin’s patented Flash Streamer technology, which removes the virus, can strongly contribute to reducing the risk of respiratory virus transmission.

Efficient against allergens as recognized by BAF (British Allergy Foundation)

The Allergy UK Seal of Approval reassures that the product is efficient at reducing small particulates which may include allergens, bacteria and viruses.

Approved allergy-friendly quality of this product/service is certified by the European Centre for Allergy Research Foundation​

An independent advisory panel of 15 leading international scientists and technicians has developed the criteria ECARF uses to  evaluate different product groups. They include threshold values and exclusion criteria that make an allergic reaction very unlikely. The criteria are regularly updated to reflect the latest scientific findings. A product receives the Seal when it can be proved through audits or studies that the criteria have been fulfilled. The Daikin Air Purifiers passed these tests and can be considered as allergy-friendly. ​

*Daikin device MCK55WVM (commercial name MCK55W), tested by Institut Pasteur de Lille, removes 99.996 % of Human Coronavirus HCoV-229E in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal). Human Coronavirus HCoV-229E is different from the virus responsible for COVID-19, SARS-CoV-2, but belongs to the same family of coronaviruses. | Daikin device MC55WVM (commercial names MC55W/VB), tested by Institut Pasteur de Lille, removes 99.98 % of Human Coronavirus HCoV-229E in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 1.4 m3, no air renewal). Human Coronavirus HCoV-229E is different from the virus responsible for COVID-19, SARS-CoV-2, but belongs to the same family of coronaviruses. | Daikin device MCK55WVM (commercial name MCK55W), tested by Institut Pasteur de Lille, removes 99.986 % of Influenza A virus subtype H1N1 in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal). | Daikin device MC55WVM (commercial names MC55W/VB), tested by Institut Pasteur de Lille, removes 99.93 % of Influenza A virus subtype H1N1 in 2.5 minutes running time at ‘turbo’ speed in laboratory conditions (air-tight chamber with inner volume 0.47 m3, no air renewal).

No maintenance costs for at least 10 years

No need to change the filters in the first 10 years after unit purchase, avoiding additional costs for regular filter changes.

One of the most silent air purifier range on the European market

Our air purifiers are whisper quiet during quiet operation (sound pressure level: 19 dBA), providing you pure air without noticing.

Compact & performing

Small size, but also perfect for very large surfaces.

FAQ

The air we breathe at home or indoors is up to 5 times more polluted than the air outside. Thanks to its unique “catch & clean” approach, the Daikin air purifier captures and removes pollutants, reducing indoor pollution and improving the quality of the air in your home, office, shop, etc.​

The Daikin air purifier helps us breathe clean air by essential reduction of viruses, fine dust and allergens. According to tests performed in the laboratories of the Institut Pasteur de Lille, Daikin air purifiers remove at least 99,98% of the human coronavirus HCoV-229E in 2.5 minutes. This virus is of the same family as SARS-CoV-2, the coronavirus behind the COVID-19 pandemic. Daikin air purifiers also helping us to prevent allergies as recognized for example by the reputed British Allergy Foundation. The deodorising filter of Daikin air purifiers successfully captures and absorbs odours wherever it’s needed.

 

The Daikin air purifier is equipped with an advanced filter system that captures viruses, bacteria and allergens meanwhile its patented Streamer technology takes care of removing it and keeping both the indoor air and the air purifier filters clean. The prefilter captures larger particles, trapping them inside. Thanks to its electrostatic capacity, Daikin HEPA filter catches pollutants without clogging the mesh, meaning that it does not need to be replaced for 10 years. The deodorising filter captures and absorbs odours without becoming saturated as happens with traditional activated carbon filters. Finally, the humidifier filter (exclusive to Daikin air purifier model equipped with humidifier) ​​eliminates bacteria in the water tank thanks to the double layer filter with silver ion cartridge. ​

 

Yes, the Daikin air purifier has been tested and certified by the prestigious ECARF institute as an ideal product for people with allergies. Above that the Daikin Air purifier is also recognized as efficient by BAF (British Allergy Foundation). This seal reassures that the product is efficient at reducing small particles which may include allergens, bacteria and viruses.

No, the Daikin Air Purifiers range is recognised as one of the most silent on the market. They are whisper quiet during silent operation mode, providing you with pure air without even noticing. ​

Opposed to other brands, it is not necessary to change a filter of the Daikin Air Purifier in the first 10 years after purchase. Giving you years of clean air with peace of mind.

Thanks to its compact design you can easily pick up and move your Air Purifier to another location. Bad smell in the kitchen? Move your Air Purifier there and let its magic work. Left the window open during Pollen season? Move your Air purifier and get rid of these pollutants in a matter of minutes.

Of course there are. Take a look through our different ranges of Air Purifiers, all with a different applicable room area.

How do our Air Purifiers provide these benefits?

Daikin unique's Catch & Clean approach 3 steps to decompose harmful substances

Couple with baby

Breathe in air that is clean and healthy

Daikin air purifiers minimise asthma and allergy symptoms by removing dust particles and pollen from your air, and keep you healthy by filtering airborne bacteria and viruses.

Mother and daughter in door

Keep your air fresh

Our air purifiers control odours, so that your home always smells fresh and clean.

Father and child in sofa

Keeping indoor air fresh is vital for your health

According to Allergy Uk, people today spend on average 90% of their time indoors. So good indoor Air quality is crucial for our health.

Pure indoor air is especially important for vulnerable groups, such as the very young & the very old, as well as people living with respiratory diseases and allergies.

bg-image

Keep your air smelling fresh

Our air purifiers control odours so that your home smells fresh and clean. Daikin's Air Purifier is designed to deal with harmful particles, as well as dust, odours, bacteria, pet hairs, moulds, pollen, mited and other allergens, leaving the indoor air clean and healthy.

Connect with healthier air

The new air purifier units MCK70Z & MC80Z come with integration to the Daikin Onecta App. This means that now you can enjoy the comfort of healthier air for you and your loved ones at the tip of fingertips.

Thanks to Daikin Onecta App, you can control, monitor & schedule your air purification operation through your smartphone.

The constant monitoring will also provide you with the much- needed peace of mind and reassure you that you are always breathier healthier.

This means, total comfort and great indoor air quality.

1 Powerful suction

Takes in air over a wide area from 3 directions.

 

 

Powerful Suction Illustration

2 Effective capturing of pollutants

Efficiently catches dust and pollutants with an electrostatic HEPA filter.

Electrostatic HEPA Filter

3 Decomposition

Uses Daikin's Streamer technology to decompose, by oxidation, harmful substances caught on the filter.*

Streamer

 

* Substances including viruses1, bacteria2, pollen3, mould spores4

Note:
1 Testing organization: Kitasato Research Center for Environmental Science; Test result certificate 21_0026 (issued by same organization); Result of experiment: 99.9% removal of A-H1N1 virus after 1 hour.
2 Testing organization: Japan Food Research Laboratories. Test number: 15044988001-0201. Test method: Attached a test piece inoculated with bacteria liquid on the upstream side of a dust collection filter installed in an air purifier, and operated it in a test area of 25 m³. Counted the number of live bacteria after five hours. Test result: Reduced by more than 99% in five hours. Test unit: Tested with MCK55S (Japanese model), a model equivalent to MCK55W series (turbo operation).
3 Various allergens were irradiated by streamer discharge and the breakdown of protein in the allergens was verified using the ELISA method, cataphoresis, or an electron microscope (Joint research with Wakayama Medical University). Test example: ‘Japanese cedar pollen Cryj-1’; Test result: 99,6% or more decomposed and removed in 2 hours.
4 Testing organization: Japan Food Research Laboratories. Test number: 204041635-001. Test result: 99.9% or more of mould (Cladosporium) spores decomposed and removed in 24 hours.

 

Humidifying Function Illustration

 

Powerful humidification to protect against air dryness and viruses

  • Protects the skin, the throat and the nostrils from dryness. 
  • Protects against viruses by maintaining appropriate humidity of the room. 
  • Maintains comfortable room humidity levels (40 to 60% RH)
  • Streamer eliminates bacteria on the humidifying filter. 

High Performance HEPA filter to catch fine particles of dust

Removes 99% of particles between 0.1μm and 2.5μm in size

The filter collects dust efficiently with electrostatic forces. It is not prone to clogging compared with non-electrostatic HEPA filters which collect particles only by the fineness of the mesh.

 

Electrostatically Charged

Electrostatic HEPA filter

Removes 99,97% of fine particles of 0,3μm Filter fiber itself is charged with static electricity, and collects particles efficiently. Doesn’t clog easily, hence causes low pressure loss.

Therefore, a larger amount of air can pass through the filter.

 

 

 

 

 

 

VS

 

 

 

The filter can purify a larger amount of air!

 

 

 

 

Electrostatically Neutral

Non-electrostatic filter

Because it catches particles relying only on mesh size, it is necessary to make mesh finer, making it easy to be clogged and cause high pressure loss.

Compact, effective and quiet thanks to the new, innovative structure

Air Purifier Structure Illustration

Daikin Air Purifiers are equipped with Streamer technology​

Explore our Air Purifiers

  • Streamer technology air purifier MC30Y

    The MC30Y Air Purifier filters out airborne particles that van often pose serious health risks. Compact and performing, up to 46 m².

  • Streamer technology air purifier MC55W

    Our streamer technology filters out airborne particles that can often pose serious health risks.

  • Ururu air purifier with Streamer MCK55W

    The Daikin Ururu air purifier MCK55W purifies and moisturises the air inside your home. Simply fill the 2.7l tank occasionally and it will humidify your room with a maximum rate of 500ml/h.

  • Ururu air purifier with streamer MCK70YV

    The Daikin Ururu air purifier MCK70YV purifies and moisturises the air inside your home. It will humidfy your room with a maximum rate of 650 ml/h, so perfect for an extended surface area.

     

  • MC80Z

    Intelligent Air Purification with minimalistic design

    The wifi-enabled Daikin MC80Z provides clean air in large spaces up to 124 m². You can simply control your indoor air quality with your smartphone through the Daikin Onecta App. 

     

  • MCK70ZH

    Intelligent Air Purification with humidification with minimalistic design

    The wifi-enabled Daikin MCK70Z gives you clean, moisturised air, purifying large spaces up to 96 m². Control your indoor air quality with your smartphone through Daikin Onecta App.

    Available in two colors: Black & Gray.

     

bg-image

Indoor Air Quality, A Daikin Experience

Find more information

Download Pricelist

Need help?

Find more information

Download Pricelist

Need help?

Find more information

Download Pricelist

Need help?

Find more information

Download Pricelist

Need help?