Seasonal Inverter
| In line with technological advancements and stricter environmental legislation, Daikin is committed to leading the way in energy-efficient residential and commercial cooling solutions.
A good example of this is Daikin’s Sky Air® Seasonal Inverter, the first on the market to anticipate Europe’s new stricter environmental requirements. A bit of background: Europe has set severe targets for energy efficiency and environmental impact to be reached by 2020. In line with these goals, more accurate rating of the real-life energy efficiency of systems will be required from 2013. This improved efficiency rating, referred to as ‘seasonal efficiency’ or SEER, measures actual energy consumption over an entire heating or cooling season. This means that it takes into account different outdoor temperatures and the resulting required capacities. Daikin is leading the way with its Sky Air® Seasonal Inverter line. These light commercial air conditioning units are the first on the market to anticipate the more accurate seasonal efficiency criteria that will apply after 2013. | ![]() | |
![]() | Because of the optimized inverter control, the Sky Air® Seasonal Inverter performs better across the entire range of outdoor temperatures. Next to this, the auxiliary modes have been redesigned in order to reduce energy consumption when the unit is not operating (e.g. standby mode). The result: up to 20% better seasonal efficiency than the current Sky Air® Super Inverter in real-life situations, and more than 50% compared to non-inverter systems. | |
Next to its high seasonal performance, Seasonal inverter units offer an important number of features, such as:
-Capacity classes ranging from 7.1kW up to 14kW (available in single and three phase)
| ![]() | |