Daikin Altherma with heat pump convector: compact, quiet, efficient heat
Daikin Europe N.V. (16/04/2010)
Daikin's heat pump convector with interlink function addresses common problem with heating efficiency
In well-insulated new residences, a combination of underfloor heating and low temperature radiators is one of the most efficient heating solutions on the market. This solution, however, is not perfect. The low leaving water temperatures important for efficiency are adequate for floor heating, but the room radiators then need to be oversized in order to emit the proper levels of heat at these low water temperatures. Adding fan coils is not always an option due to noise levels. Plus radiators have no cooling function. To address all these issues, Daikin Europe N.V. announces a Heat Pump Convector solution with interlink function.
Heat Pump Convector: small, quiet, quick, and efficient
The Heat Pump Convector is able to emit the required levels of heat at low leaving water temperatures, while retaining a modest size. The units are able to quickly heat up a room and are inaudible (down to 18 dBA or 12 dBA depending on model and fan speed), making them also ideal for bedrooms. A handy remote control per convector allows easy control of the unit, including room temperature, fan speed, automatic or night mode, rapid heating or cooling, and weekly timer.
Optimum water temperatures to underfloor elements and convectors
To get the most out of the Heat Pump Convectors, Daikin has developed an interlink system. Instead of the leaving water circuit being switched on and off via a thermostat in a single master room, each convector can be directly wired to the Daikin Altherma indoor unit, the system’s intelligence centre. This allows all rooms to have heat when required, regardless of the state of the other rooms. In addition to taking account of outdoor ambient temperature, it can intelligently control the leaving water temperature in function of underfloor heating demand, convector demand, or both. This increases efficiency by 25-40%, with COP’s between 3 and 4 depending on mode.
Installation flexibility
In highly insulated buildings, an optimum leaving water temperature of 35° C is suitable for the underfloor heating as well as the convectors. This is the simplest installation. In other situations, however, a two-zone solution is possible: 35° C water to the underfloor elements and 45° C to the convectors. Optimum outlet water temperature is assured in all circumstances by using the interlink system with optimised leaving water temperatures.
The ability to have two water temperature zones also increases flexibility with respect to cooling. If refurbishment projects don’t allow the installation of a drain pipe to remove condensation, a single zone solution can be chosen, with 18° C water temperature safely sent to both underfloor elements and convectors (a Daikin first), without the risk of condensation. If drain piping is possible, a two-zone solution can be applied: 18° C to the underfloor elements and 7° C to the convectors.
Daikin Europe N.V.’s Heat Pump Convector solution is available for Daikin Altherma and Heat Pump Chiller solutions. For more information on these and the complete range of ultra-efficient Daikin residential heating and cooling solutions, visit www.daikin.eu.
--------------
Daikin Altherma with heat pump convector: compact, quiet, efficient heat
Improving on a good thing
In well-insulated new residences, a combination of under floor heating and low temperature radiators is one of the most cost-effective heating solutions on the market. Until now, however, such systems required bulky, oversized radiators in the individual rooms. This was because the low leaving water temperatures important for efficiency are adequate for floor heating, but not for normal sized room radiators. Smaller solutions such as traditional convectors often entailed unacceptable noise levels. What’s more, radiators have no cooling function.
To address these issues, Daikin Europe N.V. announces a heat pump convector solution with interlink function for its Daikin Altherma residential heating system.
Quick heating and cooling of individual rooms in a compact, whisper quiet package
Daikin heat pump convectors emit the required levels of heat at efficient low leaving water temperatures, while retaining a modest size and quiet operation. They can quickly heat up or cool a room and are inaudible (down to 19 dBA – comparable to rustling leaves – depending on model and fan speed), making them also ideal for bedrooms.
25-40% reduction in heating costs by interlink function
To get the most out of the heat pump convectors, each convector can be directly connected to the Daikin indoor unit or Daikin Altherma Low Temperature Monobloc, the system’s intelligence centre. The leaving water temperature can then be intelligently controlled depending on under floor heating demand, heat pump convector demand, or both. Plus, unlike traditional systems with the water temperature determined by a single master room, all rooms can have maximum heat when required, regardless of the state of the other rooms. A handy remote control per heat pump convector allows easy control of the unit, including room temperature, fan speed, automatic or night mode, rapid heating or cooling, and weekly timer.
Optimal control of leaving water temperatures not only means increased comfort. Efficiency gains of 25-40%, with COP’s (coefficient of performance) between 3 and 4, are possible depending on the mode. Daikin Altherma with a heat pump convector also supports cooling, for optimum room comfort regardless of season.
Daikin’s heat pump convector solution is optimized for Daikin Altherma solutions, but will of course work with any hydronic heating or cooling source, such as minichiller or boilers.
For more information on these and the complete range of ultra-efficient Daikin residential heating and cooling solutions, visit www.daikin.eu.